JSON data types. More...

Data Structures

struct gos_json_tok_t
Parse JSON token. More...
struct gos_json_parse_config_t
JSON parser configuration. More...

Typedefs

typedef void * gos_json_parse_context_t
Context of JSON parsing.
typedef gos_result_t (* gos_json_parse_reader_t ) (void *user, void *data, uint32_t max_length, uint32_t *bytes_read)
Reader callback. More...
typedef gos_result_t (* gos_json_token_callback_t ) (void *user, gos_json_parse_context_t *context, gos_json_tok_t *tok)
Allocate token callback. More...

Enumerations

enum gos_json_type_t {
GOS_JSON_TYPE_ARRAY ,
GOS_JSON_TYPE_OBJECT ,
GOS_JSON_TYPE_STRING ,
GOS_JSON_TYPE_BOOLEAN ,
GOS_JSON_TYPE_INTEGER ,
GOS_JSON_TYPE_INTEGER64 ,
GOS_JSON_TYPE_FLOAT ,
GOS_JSON_TYPE_NULL
}
JSON token type. More...
enum gos_json_parse_flag_t { JSON_FLAG_STRINGS_INLINE = (1 << 0) }

Detailed Description

JSON data types.

Typedef Documentation

◆ gos_json_parse_reader_t

typedef gos_result_t (* gos_json_parse_reader_t) (void *user, void *data, uint32_t max_length, uint32_t *bytes_read)

Reader callback.

This is an optional callback that is called to read more JSON formatted data.

If there is no more data to be read, set bytes_read to 0 which tells the parser to stop calling this callback.

Parameters
user Optional pointer to user data, passed to gos_json_parse_chunked() , leave NULL if unused
data Buffer to hold read data
max_length Length of given buffer
bytes_read Number of bytes actually read, set to 0 if no more data available
Returns
gos_result_t result of api call

◆ gos_json_token_callback_t

typedef gos_result_t (* gos_json_token_callback_t) (void *user, gos_json_parse_context_t *context, gos_json_tok_t *tok)

Allocate token callback.

This is called before every token is allocated. This callback should return GOS_SUCCESS if the token should be allocated, GOS_ABORTED if the token should NOT be allocated, anything else will cause the parser to fail.

Parameters
user Optional pointer to user data, passed to gos_json_parse_chunked() , leave NULL if unused
context Parser context pointer
tok The token that may be allocated
Returns
GOS_SUCCESS if token should be allocated, GOS_ABORTED if token should NOT be allocated, anything else is a failure

Enumeration Type Documentation

◆ gos_json_parse_flag_t

JSON parsing flags

Enumerator
JSON_FLAG_STRINGS_INLINE

Only reference strings in json tokens, do not create copy.

Note
: The string values will only persist for as long as the parsed buffer is valid.

◆ gos_json_type_t

JSON token type.

See this tutorial for more info.

Enumerator
GOS_JSON_TYPE_ARRAY

an ordered sequence of values

GOS_JSON_TYPE_OBJECT

an unordered collection of key:value pairs

GOS_JSON_TYPE_STRING

double-quoted Unicode with backslash escaping

GOS_JSON_TYPE_BOOLEAN

true or false

GOS_JSON_TYPE_INTEGER

32bit integer

GOS_JSON_TYPE_INTEGER64

64bit integer

GOS_JSON_TYPE_FLOAT

floating point number (returned as a string)

GOS_JSON_TYPE_NULL

empty