Stream APIs
APIs for accessing SPI master 'stream' functionality. More...
Functions |
|
| gos_result_t | gos_spi_stream_configure ( gos_spi_t port, gos_gpio_t ss_gpio, gos_spi_flag_t flags, uint32_t clock_rate) |
|
Configure SPI stream for communication with SPI slave.
More...
|
|
| gos_result_t | gos_spi_stream_open ( gos_handle_t *handle_ptr, uint16_t rx_buffer_size) |
|
Open SPI stream to slave device.
More...
|
|
| gos_result_t | gos_spi_stream_write ( gos_handle_t handle, const void *data, uint32_t size) |
|
Write data to slave device.
More...
|
|
| gos_result_t | gos_spi_stream_read ( gos_handle_t handle, void *data, uint32_t max_size, uint32_t *bytes_read_ptr) |
|
Read data from slave device.
More...
|
|
| gos_result_t | gos_spi_stream_read_with_buffer ( gos_handle_t handle, gos_buffer_t *buffer) |
|
Read SPI stream data into buffer.
More...
|
|
| gos_result_t | gos_spi_stream_close ( gos_handle_t handle) |
|
Close SPI stream.
More...
|
|
| gos_result_t | gos_spi_stream_set_slave_select ( gos_handle_t handle, gos_gpio_t ss_gpio) |
|
Switch SPI stream's slave device.
More...
|
|
Detailed Description
APIs for accessing SPI master 'stream' functionality.
Function Documentation
◆ gos_spi_stream_close()
| gos_result_t gos_spi_stream_close | ( | gos_handle_t |
handle
|
) |
Close SPI stream.
See Gecko OS Command API documentation: stream_close .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to close
- Returns
- gos_result_t result of api call
◆ gos_spi_stream_configure()
| gos_result_t gos_spi_stream_configure | ( | gos_spi_t |
port,
|
| gos_gpio_t |
ss_gpio,
|
||
| gos_spi_flag_t |
flags,
|
||
| uint32_t |
clock_rate
|
||
| ) |
Configure SPI stream for communication with SPI slave.
See Gecko OS Command API documentation: spi_master_config .
- Parameters
-
[in] portSPI peripheral port [in] ss_gpioSlave-select gpio [in] flagsConfiguration flags, see SPI_FLAG macros [in] clock_rateSPI master clock
- Returns
- result of api call, see gos_result_t
◆ gos_spi_stream_open()
| gos_result_t gos_spi_stream_open | ( | gos_handle_t * |
handle_ptr,
|
| uint16_t |
rx_buffer_size
|
||
| ) |
Open SPI stream to slave device.
See Gecko OS Command API documentation: spi_master_open .
- Parameters
-
[out] handle_ptrStream handle [in] rx_buffer_sizeSize of RX buffer
- Returns
- result of api call, see gos_result_t
◆ gos_spi_stream_read()
| gos_result_t gos_spi_stream_read | ( | gos_handle_t |
handle,
|
| void * |
data,
|
||
| uint32_t |
max_size,
|
||
| uint32_t * |
bytes_read_ptr
|
||
| ) |
Read data from slave device.
See Gecko OS Command API documentation: spi_master_open , stream_read .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [out] dataBuffer to hold read data [in] max_sizeMaximum amount of data to read [out] bytes_read_ptrPointer to hold actual amount of data read (set NULL if not used)
- Returns
- gos_result_t result of api call
◆ gos_spi_stream_read_with_buffer()
| gos_result_t gos_spi_stream_read_with_buffer | ( | gos_handle_t |
handle,
|
| gos_buffer_t * |
buffer
|
||
| ) |
Read SPI stream data into buffer.
See gos_read_with_buffer() for more information.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handleStream handle bufferBuffer to specify how much data to read, then return how much data was read with pointer to data
- Returns
- gos_result_t result of api call
◆ gos_spi_stream_set_slave_select()
| gos_result_t gos_spi_stream_set_slave_select | ( | gos_handle_t |
handle,
|
| gos_gpio_t |
ss_gpio
|
||
| ) |
Switch SPI stream's slave device.
A SPI stream can be associated with multiple SPI slaves. A SPI slave is configured with gos_spi_stream_configure() The configured SPI slave is then selected with this API
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleSPI stream handle [in] ss_gpioGPIO of configured SPI slave
- Returns
- gos_result_t result of api call
◆ gos_spi_stream_write()
| gos_result_t gos_spi_stream_write | ( | gos_handle_t |
handle,
|
| const void * |
data,
|
||
| uint32_t |
size
|
||
| ) |
Write data to slave device.
See Gecko OS Command API documentation: spi_master_open , stream_write .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [in] dataData to write to stream [in] sizeSize of data in bytes to write
- Returns
- gos_result_t result of api call