Buffered Writer
APIs for writing (i.e. packing) data into a dynamic buffer. More...
Functions |
|
| gos_result_t | gos_msgpack_buffered_writer_init ( gos_msgpack_context_t **context_ptr, uint32_t initial_length) |
| gos_result_t | gos_msgpack_buffered_writer_deinit ( gos_msgpack_context_t *context, bool free_buffer) |
| gos_result_t | gos_msgpack_buffered_writer_get_buffer (const gos_msgpack_context_t *context, gos_buffer_t *buffer) |
Detailed Description
APIs for writing (i.e. packing) data into a dynamic buffer.
Function Documentation
◆ gos_msgpack_buffered_writer_deinit()
| gos_result_t gos_msgpack_buffered_writer_deinit | ( | gos_msgpack_context_t * |
context,
|
| bool |
free_buffer
|
||
| ) |
De-allocate buffered msgpack writer context
This de-allocates the memory allocated by gos_msgpack_buffered_writer_init()
This will also optionally de-allocated the internal buffer. If the internal buffer is NOT de-allocated (e.g.
free_buffer
= false), then
gos_msgpack_buffered_writer_get_buffer()
should FIRST be used to retrieve a reference to the internal buffer.
Then at a later point,
gos_free()
should be used to de-allocate the returned
buffer.data
.
- Parameters
-
[in] contextBuffered msgpack writer context to de-allocated [in] free_bufferIf true also de-allocate internal buffer, if false internal buffer is NOT de-allocated.
◆ gos_msgpack_buffered_writer_get_buffer()
| gos_result_t gos_msgpack_buffered_writer_get_buffer | ( | const gos_msgpack_context_t * |
context,
|
| gos_buffer_t * |
buffer
|
||
| ) |
Retrieve internal buffer of buffered msgpack writer context
This retrieves the internal buffer used by a buffered msgpack writer. The
buffer.data
points to the allocated buffer. The
buffer.size
is the total amount of data written to the buffer.
- Parameters
-
[in] contextBuffered msgpack writer context [out] buffergos_buffer_t to populate with internal buffer
◆ gos_msgpack_buffered_writer_init()
| gos_result_t gos_msgpack_buffered_writer_init | ( | gos_msgpack_context_t ** |
context_ptr,
|
| uint32_t |
initial_length
|
||
| ) |
Initialize buffered msgpack writer context
This initializes a buffered msgpack writer context. Once initialized, the Write APIs may be used to populate msgpack data into the returned gos_msgpack_context_t While writing data, the internal buffer will automatically be increased as necessary.
Once all the data is populated, use gos_msgpack_buffered_writer_get_buffer() to retrieve the populated buffer.
Use gos_msgpack_buffered_writer_deinit() to cleanup the allocated gos_msgpack_context_t .
- Parameters
-
[out] context_ptrPointer to hold allocated gos_msgpack_context_t [in] initial_lengthInitial length of internal buffer, this will increase as needed
- Returns
- gos_result_t , result of API