Queue
RTOS queue functions. More...
Functions |
|
| gos_result_t | gos_rtos_queue_init (gos_queue_t *queue, uint32_t message_size, uint32_t number_of_messages) |
|
Initializes a queue.
More...
|
|
| gos_result_t | gos_rtos_queue_deinit (gos_queue_t *queue) |
|
De-initialise a queue.
More...
|
|
| gos_result_t | gos_rtos_queue_push (gos_queue_t *queue, const void *message, uint32_t timeout_ms) |
|
Push an object onto the back of a queue.
More...
|
|
| gos_result_t | gos_rtos_queue_push_to_front (gos_queue_t *queue, const void *message, uint32_t timeout_ms) |
|
Push an object onto the front of a queue.
More...
|
|
| gos_result_t | gos_rtos_queue_pop (gos_queue_t *queue, void *message, uint32_t timeout_ms) |
|
Pops an object off a queue.
More...
|
|
| gos_result_t | gos_rtos_queue_flush (gos_queue_t *queue) |
|
Remove all objects from the queue.
More...
|
|
| gos_result_t | gos_rtos_queue_get_count (gos_queue_t *queue, uint32_t *count_ptr) |
|
Get number of elements in queue.
More...
|
|
| gos_result_t | gos_rtos_queue_is_empty (gos_queue_t *queue) |
|
Check if a queue is empty.
More...
|
|
| gos_result_t | gos_rtos_queue_is_full (gos_queue_t *queue) |
|
Check if a queue is full.
More...
|
|
Detailed Description
RTOS queue functions.
Function Documentation
◆ gos_rtos_queue_deinit()
| gos_result_t gos_rtos_queue_deinit | ( | gos_queue_t * |
queue
|
) |
De-initialise a queue.
Deletes a queue created with gos_rtos_queue_init()
- Parameters
-
[in] queue: Pointer to the queue handle
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_flush()
| gos_result_t gos_rtos_queue_flush | ( | gos_queue_t * |
queue
|
) |
Remove all objects from the queue.
This clears all message from the queue.
- Parameters
-
[in] queue: Pointer to the queue handle
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_get_count()
| gos_result_t gos_rtos_queue_get_count | ( | gos_queue_t * |
queue,
|
| uint32_t * |
count_ptr
|
||
| ) |
Get number of elements in queue.
Return the number of messages currently in the queue.
- Parameters
-
[in] queue: Pointer to the queue handle [out] count_ptr: Pointer to hold number of message in queue
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_init()
| gos_result_t gos_rtos_queue_init | ( | gos_queue_t * |
queue,
|
| uint32_t |
message_size,
|
||
| uint32_t |
number_of_messages
|
||
| ) |
Initializes a queue.
Initialises a FIFO queue
- Parameters
-
[in] queue: Pointer to the queue handle to be initialised [in] message_size: Size in bytes of objects that will be held in the queue [in] number_of_messages: Depth of the queue - i.e. max number of objects in the queue
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_is_empty()
| gos_result_t gos_rtos_queue_is_empty | ( | gos_queue_t * |
queue
|
) |
Check if a queue is empty.
This returns GOS_SUCCESS if the queue is empty. It returns GOS_ERROR if the queue is NOT empty.
- Parameters
-
[in] queue: Pointer to the queue handle
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_is_full()
| gos_result_t gos_rtos_queue_is_full | ( | gos_queue_t * |
queue
|
) |
Check if a queue is full.
This returns GOS_SUCCESS if the queue is full. It returns GOS_ERROR if the queue is NOT full.
- Parameters
-
[in] queue: Pointer to the queue handle
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_pop()
| gos_result_t gos_rtos_queue_pop | ( | gos_queue_t * |
queue,
|
| void * |
message,
|
||
| uint32_t |
timeout_ms
|
||
| ) |
Pops an object off a queue.
This removes an object from the front of the queue. i.e. The oldest object in the queue is removed.
If the queue is empty, this will block until an object is added to the queue OR the specified
timeout_ms
is exceeded.
- Parameters
-
[in] queue: Pointer to the queue handle [out] message: Pointer to a buffer that will receive the object being popped off the queue. Size is assumed to be the size specified in gos_rtos_queue_init() , hence you must ensure the buffer is long enough or memory corruption will result [in] timeout_msNumber of milliseconds to wait before returning
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_push()
| gos_result_t gos_rtos_queue_push | ( | gos_queue_t * |
queue,
|
| const void * |
message,
|
||
| uint32_t |
timeout_ms
|
||
| ) |
Push an object onto the back of a queue.
Pushes an object to the back of a queue. This pushed object will be the last to be removed with gos_rtos_queue_pop()
If the queue is full, this API will block until room is available in the queue OR the specified
timeout_ms
is exceeded.
- Parameters
-
[in] queue: Pointer to the queue handle [in] message: Object to be added to the queue. Size is assumed to be the size specified in gos_rtos_queue_init() [in] timeout_ms: Number of milliseconds to wait before returning
- Returns
- Result of API call, gos_result_t
◆ gos_rtos_queue_push_to_front()
| gos_result_t gos_rtos_queue_push_to_front | ( | gos_queue_t * |
queue,
|
| const void * |
message,
|
||
| uint32_t |
timeout_ms
|
||
| ) |
Push an object onto the front of a queue.
Pushes an object to the front of a queue. This pushed object will be the first to be removed with gos_rtos_queue_pop()
If the queue is full, this API will block until room is available in the queue OR the specified
timeout_ms
is exceeded.
- Parameters
-
[in] queue: Pointer to the queue handle [in] message: Object to be added to the queue. Size is assumed to be the size specified in gos_rtos_queue_init() [in] timeout_ms: Number of milliseconds to wait before returning
- Returns
- Result of API call, gos_result_t