Data types for web setup. More...

Typedefs

typedef void(* gos_setup_client_event_t ) (const gos_softap_client_t *client)
Setup client event handler prototype. More...

Enumerations

enum gos_setup_os_type_t {
GOS_SETUP_OS_INVALID ,
GOS_SETUP_OS_UNKNOWN ,
GOS_SETUP_OS_WINDOWS ,
GOS_SETUP_OS_WINDOWS_MOBILE ,
GOS_SETUP_OS_ANDROID ,
GOS_SETUP_OS_LINUX ,
GOS_SETUP_OS_CHROME ,
GOS_SETUP_OS_IPHONE ,
GOS_SETUP_OS_IPOD ,
GOS_SETUP_OS_IPAD ,
GOS_SETUP_OS_MAC ,
GOS_SETUP_OS_BLACKBERRY ,
GOS_SETUP_OS_SYMBIAN
}

Detailed Description

Data types for web setup.

Typedef Documentation

◆ gos_setup_client_event_t

typedef void(* gos_setup_client_event_t) (const gos_softap_client_t *client)

Setup client event handler prototype.

This handler is registered with gos_setup_register_client_event_handler() . This handler is called when a client connects to the setup softap AND when the client connects to the HTTP server.

The 'additional' member of gos_softap_client_t contains the client's operating system type, gos_setup_os_type_t . When first connecting the OS type is GOS_SETUP_OS_INVALID . Once the client connects to the HTTP server, the OS type is determined.

Parameters
info Struct contain information about client. gos_softap_client_t

Enumeration Type Documentation

◆ gos_setup_os_type_t

The setup client's operating system type

The OS is supplied by the client when it connects to the device's HTTP server. A client's OS type is GOS_SETUP_OS_INVALID until the client connects.

Enumerator
GOS_SETUP_OS_INVALID

GOS_SETUP_OS_INVALID.

GOS_SETUP_OS_UNKNOWN

GOS_SETUP_OS_UNKNOWN.

GOS_SETUP_OS_WINDOWS

GOS_SETUP_OS_WINDOWS.

GOS_SETUP_OS_WINDOWS_MOBILE

GOS_SETUP_OS_WINDOWS_MOBILE.

GOS_SETUP_OS_ANDROID

GOS_SETUP_OS_ANDROID.

GOS_SETUP_OS_LINUX

GOS_SETUP_OS_LINUX.

GOS_SETUP_OS_CHROME

GOS_SETUP_OS_CHROME.

GOS_SETUP_OS_IPHONE

GOS_SETUP_OS_IPHONE.

GOS_SETUP_OS_IPOD

GOS_SETUP_OS_IPOD.

GOS_SETUP_OS_IPAD

GOS_SETUP_OS_IPAD.

GOS_SETUP_OS_MAC

GOS_SETUP_OS_MAC.

GOS_SETUP_OS_BLACKBERRY

GOS_SETUP_OS_BLACKBERRY.

GOS_SETUP_OS_SYMBIAN

GOS_SETUP_OS_SYMBIAN.