Configuration
Chip configuration APIs. More...
Functions |
|
| gos_result_t | gos_atca_lock_data_zone (void) |
| gos_result_t | gos_atca_data_zone_is_locked (bool *is_locked) |
| gos_result_t | gos_atca_write_data_zone (uint16_t slot_id, const void *data, uint32_t length) |
| gos_result_t | gos_atca_read_data_zone (uint16_t slot_id, void *data, uint32_t length) |
| gos_result_t | gos_atca_lock_config_zone (void) |
| gos_result_t | gos_atca_config_zone_is_locked (bool *is_locked) |
| gos_result_t | gos_atca_write_config_zone (const void *config) |
| gos_result_t | gos_atca_read_config_zone (void *config) |
| gos_result_t | gos_atca_compare_config_zone (const void *expected_config, bool *is_same_config) |
Detailed Description
Chip configuration APIs.
Function Documentation
◆ gos_atca_compare_config_zone()
| gos_result_t gos_atca_compare_config_zone | ( | const void * |
expected_config,
|
| bool * |
is_same_config
|
||
| ) |
Compares a specified configuration zone with the configuration zone currently on the SE
This only compares the static portions of the configuration zone and skips those that are unique per SE (first 16 bytes) and areas that can change after the configuration zone has been locked (e.g. LastKeyUse).
- Parameters
-
[in] expected_configFull configuration data to compare the SE against [out] is_same_configResult is returned here. True if the static portions on the configuration zones are the same
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/se_utils.c .
◆ gos_atca_config_zone_is_locked()
| gos_result_t gos_atca_config_zone_is_locked | ( | bool * |
is_locked
|
) |
Executes Read command, which reads the configuration zone to see if the specified zone is locked
- Parameters
-
[out] is_lockedLock state returned here. True if locked
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/se_utils.c .
◆ gos_atca_data_zone_is_locked()
| gos_result_t gos_atca_data_zone_is_locked | ( | bool * |
is_locked
|
) |
Executes Read command, which reads the data zone to see if the specified zone is locked.
- Parameters
-
[out] is_lockedLock state returned here. True if locked.
- Returns
- gos_result_t result of API
◆ gos_atca_lock_config_zone()
| gos_result_t gos_atca_lock_config_zone | ( | void |
|
) |
Unconditionally (no CRC required) lock the config zone
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/se_utils.c .
◆ gos_atca_lock_data_zone()
| gos_result_t gos_atca_lock_data_zone | ( | void |
|
) |
Unconditionally (no CRC required) lock the data zone (slots and OTP).
ConfigZone must be locked and DataZone must be unlocked for the zone to be successfully locked.
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/se_utils.c .
◆ gos_atca_read_config_zone()
| gos_result_t gos_atca_read_config_zone | ( | void * |
config
|
) |
Executes Read command to read the complete SE configuration zone
- Parameters
-
[out] configonfiguration zone data is returned here. 128 bytes for ATECC
- Returns
- gos_result_t result of API
◆ gos_atca_read_data_zone()
| gos_result_t gos_atca_read_data_zone | ( | uint16_t |
slot_id,
|
| void * |
data,
|
||
| uint32_t |
length
|
||
| ) |
Used to read an arbitrary number of bytes from data zone configured for clear reads
This function will issue the Read command as many times as is required to read the requested data.
- Parameters
-
[in] slot_idSlot number to read from [out] dataRead data is returned here [in] lengthNumber of bytes to read starting from the offset
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/commands.c , and demo/secure_element/se_utils.c .
◆ gos_atca_write_config_zone()
| gos_result_t gos_atca_write_config_zone | ( | const void * |
config
|
) |
Executes the Write command, which writes the configuration zone
First 16 bytes are skipped as they are not writable. LockValue and LockConfig are also skipped and can only be changed via the Lock command.
This API may fail if UserExtra and/or Selector bytes have already been set to non-zero values.
- Parameters
-
[in] configData to the config zone data. This should be 128 bytes for ECC.
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/se_utils.c .
◆ gos_atca_write_data_zone()
| gos_result_t gos_atca_write_data_zone | ( | uint16_t |
slot_id,
|
| const void * |
data,
|
||
| uint32_t |
length
|
||
| ) |
Executes the Write command, which writes data into the data zone with a given byte offset and length. Offset and length must be multiples of a word (4 bytes).
If data zone is unlocked, only 32-byte writes are allowed to slots and the offset and length must be multiples of 32 or the write will fail.
- Parameters
-
[in] slot_idthe slot number to write to [in] dataData to be written [in] lengthNumber of bytes to be written. Must be a multiple of a word (4 bytes)
- Returns
- gos_result_t result of API
- Examples:
- demo/secure_element/commands.c .