Api_system_shutdown

Data Structures

struct gos_shutdown_options_t

Functions

gos_result_t gos_shutdown (const gos_shutdown_options_t *options)
Put module into shutdown mode. More...

Detailed Description

Function Documentation

◆ gos_shutdown()

gos_result_t gos_shutdown ( const gos_shutdown_options_t * options )

Put module into shutdown mode.

In shutdown mode there is no RAM retention. Upon wakeup the device reboots into its reset state.

See Gecko OS Command API documentation: shutdown .

Note
Leave the options argument NULL to use the configured Gecko OS settings
Parameters
[in] options Options for how the device should wakeup, see gos_shutdown_options_t , leave NULL to use configured Gecko OS settings
Returns
gos_result_t result of API