gos_hs_tls_client_t Struct Reference

Information about connected TLS clients. More...

Data Fields

struct gos_hs_tls_client * next
Pointer to next client in list.
uint64_t timestamp
Timestamp of last time client has accessed the HTTP server.
char common_name [1]
The 'Common Name' of the client's TLS certificate.

Detailed Description

Information about connected TLS clients.

This contains information about TLS clients that have connected to the HTTP server.

This is only used when client TLS authentication is used.

More info here: Secure HTTPS Server