UDP Client/Server
UDP client/server functions. More...
Modules |
|
| Types | |
|
UDP client/server data types.
|
|
Functions |
|
| gos_result_t | gos_udp_connect (const char *host, uint16_t remote_port, uint16_t local_port, gos_handle_t *handle_ptr) |
|
Connect to remote UDP server.
More...
|
|
| gos_result_t | gos_udp_connect_with_config (const gos_udp_client_config_t *config, gos_handle_t *handle_ptr) |
|
Connect to remote UDP server.
More...
|
|
| gos_result_t | gos_udp_listen ( gos_interface_t interface, uint16_t local_port, gos_handle_t *handle_ptr) |
|
Start UDP server.
More...
|
|
| gos_result_t | gos_udp_stop_listening (void) |
|
Stop UDP server on specified interface.
More...
|
|
| gos_result_t | gos_udp_read ( gos_handle_t handle, void *data, uint32_t max_size, uint32_t *bytes_read_ptr) |
|
Read UDP stream data.
More...
|
|
| gos_result_t | gos_udp_read_with_buffer ( gos_handle_t handle, gos_buffer_t *buffer) |
|
Read UDP stream data into buffer.
More...
|
|
| gos_result_t | gos_udp_write ( gos_handle_t handle, const void *data, uint32_t size) |
|
Write UDP stream data.
More...
|
|
| gos_result_t | gos_udp_close ( gos_handle_t handle) |
|
Close UDP stream.
More...
|
|
| gos_result_t | gos_udp_poll ( gos_handle_t handle, uint32_t *rx_bytes_available, uint32_t *tx_bytes_available) |
|
Poll UDP stream for RX data.
More...
|
|
| gos_result_t | gos_udp_query (uint32_t *client_ip, uint16_t *client_port) |
|
Get current UDP server client info.
More...
|
|
| gos_result_t | gos_udp_sendto (const void *data, uint32_t size, const char *host, uint16_t port) |
|
Send data to specific remote IP address/port.
More...
|
|
| gos_result_t | gos_udp_receivefrom ( gos_buffer_t *data_buffer, const char *host, uint16_t remote_port, uint32_t timeout) |
|
Receive data from specific remote host/port.
More...
|
|
| gos_result_t | gos_udp_register_receive_event_handler ( gos_handle_t handle, gos_stream_event_handler_t receive_handler) |
|
Register UDP data received event handler.
More...
|
|
Detailed Description
UDP client/server functions.
Function Documentation
◆ gos_udp_close()
| gos_result_t gos_udp_close | ( | gos_handle_t |
handle
|
) |
Close UDP stream.
See Gecko OS Command API documentation: stream_close .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to close
- Returns
- gos_result_t result of api call
- Examples:
- network/udp_hello_gpio/main.c , and test/throughput/main.c .
◆ gos_udp_connect()
| gos_result_t gos_udp_connect | ( | const char * |
host,
|
| uint16_t |
remote_port,
|
||
| uint16_t |
local_port,
|
||
| gos_handle_t * |
handle_ptr
|
||
| ) |
Connect to remote UDP server.
See Gecko OS Command API documentation: udp_client .
- Parameters
-
[in] hostRemote UDP server host or IP address [in] remote_portRemote UDP server port [in] local_portLocal UDP port, set to 0 to use any available port [out] handle_ptrUDP stream handle
- Returns
- gos_result_t result of API
- Examples:
- network/udp_client/main.c , network/udp_hello_gpio/main.c , and test/throughput/main.c .
◆ gos_udp_connect_with_config()
| gos_result_t gos_udp_connect_with_config | ( | const gos_udp_client_config_t * |
config,
|
| gos_handle_t * |
handle_ptr
|
||
| ) |
Connect to remote UDP server.
See Gecko OS Command API documentation: udp_client .
- Parameters
-
[in] configConnection configuration, see gos_udp_client_config_t [out] handle_ptrUDP stream handle
- Returns
- gos_result_t result of API
◆ gos_udp_listen()
| gos_result_t gos_udp_listen | ( | gos_interface_t |
interface,
|
| uint16_t |
local_port,
|
||
| gos_handle_t * |
handle_ptr
|
||
| ) |
Start UDP server.
See Gecko OS Command API documentation: udp_server start .
- Parameters
-
[in] interfaceInterface to start server, see gos_interface_t [in] local_portPort for server to listen [out] handle_ptrUDP stream handle
- Returns
- gos_result_t result of API
- Examples:
- test/throughput/main.c .
◆ gos_udp_poll()
| gos_result_t gos_udp_poll | ( | gos_handle_t |
handle,
|
| uint32_t * |
rx_bytes_available,
|
||
| uint32_t * |
tx_bytes_available
|
||
| ) |
Poll UDP stream for RX data.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleHandle of stream to poll [out] rx_bytes_availablePointer to hold number of bytes available to read [out] tx_bytes_availablePointer to hold available TX buffer space
- Returns
- gos_result_t result of api call
- Examples:
- network/udp_client/main.c .
◆ gos_udp_query()
| gos_result_t gos_udp_query | ( | uint32_t * |
client_ip,
|
| uint16_t * |
client_port
|
||
| ) |
Get current UDP server client info.
See Gecko OS Command API documentation: udp_server read -q .
- Parameters
-
[out] client_ipIPv4 address of client [out] client_portClient remote port
- Returns
- gos_result_t result of api call
◆ gos_udp_read()
| gos_result_t gos_udp_read | ( | gos_handle_t |
handle,
|
| void * |
data,
|
||
| uint32_t |
max_size,
|
||
| uint32_t * |
bytes_read_ptr
|
||
| ) |
Read UDP stream data.
See Gecko OS Command API documentation: stream_read .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [out] dataBuffer to hold read data [in] max_sizeMaximum amount of data to read [out] bytes_read_ptrPointer to hold actual amount of data read (set NULL if not used)
- Returns
- gos_result_t result of api call
- Examples:
- test/throughput/main.c .
◆ gos_udp_read_with_buffer()
| gos_result_t gos_udp_read_with_buffer | ( | gos_handle_t |
handle,
|
| gos_buffer_t * |
buffer
|
||
| ) |
Read UDP stream data into buffer.
See gos_read_with_buffer() for more information.
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
handleStream handle bufferBuffer to specify how much data to read, then return how much data was read with pointer to data
- Returns
- gos_result_t result of api call
- Examples:
- network/udp_client/main.c .
◆ gos_udp_receivefrom()
| gos_result_t gos_udp_receivefrom | ( | gos_buffer_t * |
data_buffer,
|
| const char * |
host,
|
||
| uint16_t |
remote_port,
|
||
| uint32_t |
timeout
|
||
| ) |
Receive data from specific remote host/port.
See gos_read_with_buffer() for details on how the data_buffer argument is used.
See Gecko OS Command API documentation: udp_server write
- Parameters
-
[in,out] data_bufferBuffer to specify how much data to read, then return how much data was read with pointer to data [in] hostRemote client host or IPv4 address [in] remote_portPort of remote client [in] timeoutMaximum time in milliseconds to wait for RX data
- Returns
- gos_result_t result of api call
◆ gos_udp_register_receive_event_handler()
| gos_result_t gos_udp_register_receive_event_handler | ( | gos_handle_t |
handle,
|
| gos_stream_event_handler_t |
receive_handler
|
||
| ) |
Register UDP data received event handler.
The registers a receive handler for either a UDP client or server.
- Note
- The event handler executes in the app Thread context
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle or UDP client or server [in] receive_handlerHandler to be issued when UDP client/server has data to be read
- Returns
- gos_result_t result of api call
- Examples:
- network/udp_client/main.c .
◆ gos_udp_sendto()
| gos_result_t gos_udp_sendto | ( | const void * |
data,
|
| uint32_t |
size,
|
||
| const char * |
host,
|
||
| uint16_t |
port
|
||
| ) |
Send data to specific remote IP address/port.
See Gecko OS Command API documentation: udp_server write
- Parameters
-
[in] dataData to send [in] sizeSize of data to send [in] hosthostname or IPv4 address of remote client [in] portClient's UDP port
- Returns
- gos_result_t result of api call
◆ gos_udp_stop_listening()
| gos_result_t gos_udp_stop_listening | ( | void |
|
) |
Stop UDP server on specified interface.
See Gecko OS Command API documentation: udp_server stop .
- Returns
- gos_result_t result of API
- Examples:
- test/throughput/main.c .
◆ gos_udp_write()
| gos_result_t gos_udp_write | ( | gos_handle_t |
handle,
|
| const void * |
data,
|
||
| uint32_t |
size
|
||
| ) |
Write UDP stream data.
See Gecko OS Command API documentation: stream_write .
- Note
- Stream handles start at 1, max handle value is GOS_MAX_STREAMS
- Parameters
-
[in] handleStream handle returned by API call [in] dataData to write to stream [in] sizeSize of data in bytes to write
- Returns
- gos_result_t result of api call
- Examples:
- network/udp_client/main.c , network/udp_hello_gpio/main.c , and test/throughput/main.c .