Contains information about a scan result. More...
Data Fields |
|
| gos_ssid_t | SSID |
|
Service Set Identification (i.e. Name of Access Point)
|
|
| gos_mac_t | BSSID |
|
Basic Service Set Identification (i.e. MAC address of Access Point)
|
|
| int16_t | signal_strength |
|
Receive Signal Strength Indication in dBm. <-90=Very poor, >-30=Excellent, 200=Off channel scan.
|
|
| uint32_t | max_data_rate |
|
Maximum data rate in kilobits/s.
|
|
| uint8_t | bss_type |
|
Network type,
gos_bss_type_t
.
|
|
| uint32_t | security |
|
Security type,
gos_security_t
.
|
|
| uint8_t | channel |
|
Radio channel that the AP beacon was received on.
|
|
| uint8_t | band |
|
Radio band,
gos_802_11_band_t
.
|
|
| uint8_t | on_channel |
|
True if scan result was recorded on the channel advertised in the packet.
|
|
| struct gos_scan_result * | next |
|
Pointer to the next scan result.
|
|
Detailed Description
Contains information about a scan result.
- Examples:
- wifi/wifi_scan/main.c .