Direct Memory Access (DMA) APIs. More...

Modules

Types
DMA data types.

Functions

gos_result_t gos_dma_alloc ( gos_handler_t callback, void *arg, gos_dma_channel_t *channel_ptr)
Allocate a DMA channel. More...
gos_result_t gos_dma_free ( gos_dma_channel_t channel)
Free a DMA channel. More...

Detailed Description

Direct Memory Access (DMA) APIs.

Function Documentation

◆ gos_dma_alloc()

gos_result_t gos_dma_alloc ( gos_handler_t callback,
void * arg,
gos_dma_channel_t * channel_ptr
)

Allocate a DMA channel.

Allocates a DMA channel from the kernel. The returned channel will be exclusively available to the user application.

Note
It is imperative to use this API to allocate channels which will be manually accessed by the application to prevent conflicts with the kernel's use of DMA.
You must use gos_dma_free() to de-allocate the channel once it is no longer needed.
Parameters
[in] callback function to be called when a DMA transfer on the channel returned by this function is complete. This function will execute in the IRQ context.
[in] arg argument to pass to callback function
[out] channel_ptr Pointer to hold channel number of allocated DMA channel
Returns
result of API call

◆ gos_dma_free()

gos_result_t gos_dma_free ( gos_dma_channel_t channel )

Free a DMA channel.

Release a channel allocated by gos_dma_alloc.

Parameters
[in] channel DMA channel to free
Returns
result of API call