Time specific types. More...

Data Structures

struct gos_iso8601_t
struct gos_iso8601_str_t

Typedefs

typedef uint32_t gos_time_t
typedef uint32_t gos_utc_seconds_t
typedef uint64_t gos_utc_ms_t
typedef int32_t gos_timezone_offset_t

Detailed Description

Time specific types.

Typedef Documentation

gos_time_t

typedef uint32_t gos_time_t

Time value in milliseconds

gos_timezone_offset_t

typedef int32_t gos_timezone_offset_t

Timezone offset in seconds

Note
This can be positive or negative

gos_utc_ms_t

typedef uint64_t gos_utc_ms_t

UTC Time in milliseconds

gos_utc_seconds_t

typedef uint32_t gos_utc_seconds_t

UTC Time in seconds