GPIO
Functions for using General Purpose Input/Output (GPIO) peripheral. More...
Modules | |
Types | |
Hardware GPIO data types. | |
Functions | |
gos_result_t | gos_gpio_init (gos_gpio_t gpio, gos_gpio_config_t direction, bool init_val) |
Initialize GPIO as input or output. More... | |
gos_result_t | gos_gpio_direct_init (gos_gpio_t gpio, gos_gpio_config_t direction) |
Initialize GPIO as input or output. More... | |
gos_result_t | gos_gpio_deinit (gos_gpio_t gpio) |
De-initialize a GPIO. This is the equivalent of using the Command API function gpio_dir with argument none More... | |
gos_result_t | gos_gpio_set (gos_gpio_t gpio, bool value) |
Set value of output GPIO (HIGH or LOW) More... | |
gos_result_t | gos_gpio_direct_set (gos_gpio_t gpio, bool value) |
Set value of output GPIO (HIGH or LOW) More... | |
bool | gos_gpio_get (gos_gpio_t gpio) |
Get value of GPIO. More... | |
gos_result_t | gos_gpio_irq_enable (gos_gpio_t gpio, gos_gpio_irq_trigger_t edge, gos_handler_t callback, void *arg) |
Execute the given callback when the specified edge event is detected on the GPIO. More... | |
gos_result_t | gos_gpio_irq_disable (gos_gpio_t gpio) |
Disables an interrupt trigger for an input GPIO pin. More... | |
gos_result_t | gos_gpio_mask_set (uint32_t gpio_mask) |
Set output GPIOs HIGH. More... | |
gos_result_t | gos_gpio_mask_clear (uint32_t gpio_mask) |
Set output GPIOs LOW. More... | |
uint32_t | gos_gpio_mask_get (uint32_t gpio_mask) |
Return value of GPIOs. More... | |
Detailed Description
Functions for using General Purpose Input/Output (GPIO) peripheral.
Function Documentation
◆ gos_gpio_deinit()
gos_result_t gos_gpio_deinit | ( | gos_gpio_t | gpio | ) |
De-initialize a GPIO. This is the equivalent of using the Command API function gpio_dir
with argument none
See Gecko OS Command API documentation: gpio_dir.
- Note
- The GPIO must be initialized with gos_gpio_init() first.
◆ gos_gpio_direct_init()
gos_result_t gos_gpio_direct_init | ( | gos_gpio_t | gpio, |
gos_gpio_config_t | direction |
||
) |
Initialize GPIO as input or output.
- Note
- This only initializes the GPIO at the hardware level. Use gos_gpio_init() for Gecko OS to be aware of this GPIO.
◆ gos_gpio_direct_set()
gos_result_t gos_gpio_direct_set | ( | gos_gpio_t | gpio, |
bool | value |
||
) |
Set value of output GPIO (HIGH or LOW)
- Note
- This bypass Gecko OS and directly accesses the GPIO driver.
◆ gos_gpio_get()
bool gos_gpio_get | ( | gos_gpio_t | gpio | ) |
Get value of GPIO.
See Gecko OS Command API documentation: gpio_set.
- Note
- The gpio need NOT be initialized as an input first.
◆ gos_gpio_init()
gos_result_t gos_gpio_init | ( | gos_gpio_t | gpio, |
gos_gpio_config_t | direction, |
||
bool | init_val |
||
) |
Initialize GPIO as input or output.
See Gecko OS Command API documentation: gpio_dir.
◆ gos_gpio_irq_disable()
gos_result_t gos_gpio_irq_disable | ( | gos_gpio_t | gpio | ) |
Disables an interrupt trigger for an input GPIO pin.
Disables an interrupt trigger for an input GPIO pin. Using this function on a gpio pin which has not been set up using gos_gpio_irq_enable() is undefined.
- Parameters
-
gpio
: the gpio pin which provided the interrupt trigger
◆ gos_gpio_irq_enable()
gos_result_t gos_gpio_irq_enable | ( | gos_gpio_t | gpio, |
gos_gpio_irq_trigger_t | edge, |
||
gos_handler_t | callback, |
||
void * | arg |
||
) |
Execute the given callback when the specified edge event is detected on the GPIO.
The callback is executed in the IRQ context and MUST be very light-weight. All heavy processing should be deferred to the app thread.
- Note
- The corresponding GPIO need MUST be configured as an input first.
- Examples:
- peripheral/gpio_irq/main.c.
◆ gos_gpio_mask_clear()
gos_result_t gos_gpio_mask_clear | ( | uint32_t | gpio_mask | ) |
Set output GPIOs LOW.
For any bit in the mask that's '1', the corresponding GPIO's value is driven LOW ('0' valued bits are ignored)
- Note
- The corresponding GPIO must be configured as an OUTPUT first.
◆ gos_gpio_mask_get()
uint32_t gos_gpio_mask_get | ( | uint32_t | gpio_mask | ) |
Return value of GPIOs.
For any bit in the mask that's '1', the corresponding GPIO's value is read and returned in the value mask.
- Note
- The corresponding GPIO need NOT be configured as an input first.
◆ gos_gpio_mask_set()
gos_result_t gos_gpio_mask_set | ( | uint32_t | gpio_mask | ) |
Set output GPIOs HIGH.
For any bit in the mask that's '1', the corresponding GPIO's value is driven HIGH ('0' valued bits are ignored)
- Note
- The corresponding GPIO must be configured as an OUTPUT first.
◆ gos_gpio_set()
gos_result_t gos_gpio_set | ( | gos_gpio_t | gpio, |
bool | value |
||
) |
Set value of output GPIO (HIGH or LOW)
- Note
- The GPIO must be initialized as an output with gos_gpio_init() first.