gos_http_request_t Struct Reference
HTTP request context. More...
Data Fields |
|
| const char * | url |
The HTTP request URL, if no schema is included
http://
is used.
|
|
| gos_tls_certificates_t | certs |
|
For HTTPS (secure) request, the TLS cert filenames,
gos_tls_certificates_t
.
|
|
| const char * | content_type |
| int32_t | content_length |
| gos_interface_t | interface |
|
Network interface,
gos_interface_t
.
|
|
| gos_http_method_t | method |
| bool | use_secure_element |
|
If true, the secure element will be used for all registered TLS operations.
|
|
Detailed Description
HTTP request context.
Field Documentation
◆ content_length
| int32_t gos_http_request_t::content_length |
Specifies the content length that will be sent. If greater/equal to zero then specifies the 'content-length' header If equal -1, then specifies 'transfer-encoding: chunked' and writes are chunked encoded
- Note
- this only used for a POST request.
◆ content_type
| const char* gos_http_request_t::content_type |
The 'content-type' header
- Note
- this only used for a POST request.
◆ method
| gos_http_method_t gos_http_request_t::method |
HTTP request method, gos_http_method_t
- Note
- This is only used for gos_http_open_request()