Data Structures | |
struct | EmberZclCommandContext_t |
Macros | |
#define | EMBER_ZCL_COMMAND_NULL ((EmberZclCommandId_t)-1) |
Typedefs | |
typedef uint8_t | EmberZclCommandId_t |
Functions | |
EmberStatus | emberZclSendDefaultResponse (const EmberZclCommandContext_t *context, EmberZclStatus_t status) |
Detailed Description
See zcl-core-types.h
for source code.
See zcl-core.h
for source code.
Macro Definition Documentation
#define EMBER_ZCL_COMMAND_NULL ((EmberZclCommandId_t)-1) |
A distinguished value that represents a null (invalid) command identifier.
Typedef Documentation
typedef uint8_t EmberZclCommandId_t |
A command identifier.
Function Documentation
EmberStatus emberZclSendDefaultResponse | ( | const EmberZclCommandContext_t * | context, |
EmberZclStatus_t | status |
||
) |
This function sends a default response to a command.
- Parameters
-
context
A command context for the response status
A status to respond with
- Returns
- EMBER_ZCL_STATUS_SUCCESS if response was sent successfully
- EMBER_ZCL_STATUS_ACTION_DENIED if response to a multicast command
- EmberStatus with failure reason otherwise