AshRxState Struct Reference
#include <
ash-v3.h
>
Data Fields | |
uint8_t | payload [MAX_ASH_PAYLOAD_SIZE ] |
uint8_t | payloadIndex |
uint8_t | escapedPayloadIndex |
uint8_t | payloadLength |
uint8_t | controlByte |
uint8_t | headerEscapeByte |
uint16_t | computedCrc |
uint8_t | highCrcByte |
uint8_t | inBetweenCrcByte |
AshRxFrameState | frameState |
bool | escapeNextByte |
The documentation for this struct was generated from the following file:
ash-v3.h