Data Structures | |
struct | EmberZclGroupEntry_t |
Macros | |
#define | EMBER_ZCL_GROUP_ALL_ENDPOINTS 0xFFFF |
#define | EMBER_ZCL_GROUP_MIN 0x0001 |
#define | EMBER_ZCL_GROUP_MAX 0xFFF7 |
#define | EMBER_ZCL_GROUP_NULL 0x0000 |
#define | EMBER_ZCL_MAX_GROUP_NAME_LENGTH 0 |
Typedefs | |
typedef uint16_t | EmberZclGroupId_t |
Functions | |
bool | emberZclIsEndpointInGroup (EmberZclEndpointId_t endpointId, EmberZclGroupId_t groupId) |
bool | emberZclGetGroupName (EmberZclEndpointId_t endpointId, EmberZclGroupId_t groupId, uint8_t *groupName, uint8_t *groupNameLength) |
EmberZclStatus_t | emberZclAddEndpointToGroup (EmberZclEndpointId_t endpointId, EmberZclGroupId_t groupId, const uint8_t *groupName, uint8_t groupNameLength) |
EmberZclStatus_t | emberZclRemoveEndpointFromGroup (EmberZclEndpointId_t endpointId, EmberZclGroupId_t groupId) |
EmberZclStatus_t | emberZclRemoveEndpointFromAllGroups (EmberZclEndpointId_t endpointId) |
EmberZclStatus_t | emberZclRemoveGroup (EmberZclGroupId_t groupId) |
EmberZclStatus_t | emberZclRemoveAllGroups (void) |
Detailed Description
See zcl-core-types.h
for source code.
See zcl-core.h
for source code.
Macro Definition Documentation
#define EMBER_ZCL_GROUP_ALL_ENDPOINTS 0xFFFF |
A group identifier for the all-endpoints (endpoint broadcast) group.
All endpoints are always members of this group. This group cannot be removed and no endpoint can be removed from it.
#define EMBER_ZCL_GROUP_MAX 0xFFF7 |
A maximum group identifier value.
#define EMBER_ZCL_GROUP_MIN 0x0001 |
A minimum group identifier value.
#define EMBER_ZCL_GROUP_NULL 0x0000 |
A distinguished value that represents a null (invalid) group identifier.
#define EMBER_ZCL_MAX_GROUP_NAME_LENGTH 0 |
Typedef Documentation
typedef uint16_t EmberZclGroupId_t |
A group identifier.
Function Documentation
EmberZclStatus_t emberZclAddEndpointToGroup | ( | EmberZclEndpointId_t | endpointId, |
EmberZclGroupId_t | groupId, |
||
const uint8_t * | groupName, |
||
uint8_t | groupNameLength |
||
) |
This function adds an endpoint to a group.
- Parameters
-
endpointId
An endpoint identifier groupId
A group identifier groupName
A pointer to an array containing name of group groupNameLength
Length of group name array (groupName is ignored if this length is 0)
- Returns
- EMBER_ZCL_STATUS_SUCCESS if the endpoint was added to the group
- EMBER_ZCL_STATUS_DUPLICATE_EXISTS if the endpoint is already a member of the group
- EMBER_ZCL_STATUS_INSUFFICIENT_SPACE if there is no capacity to store the endpoint/group association
- EMBER_ZCL_STATUS_FAILURE if groupId is EMBER_ZCL_GROUP_ALL_ENDPOINTS, or if groupId is not a value between EMBER_ZCL_GROUP_MIN and EMBER_ZCL_GROUP_MAX inclusive, or if groupNameLength is greater than EMBER_ZCL_MAX_GROUP_NAME_LENGTH, or if groupNameLength is non-zero and groupName is NULL
bool emberZclGetGroupName | ( | EmberZclEndpointId_t | endpointId, |
EmberZclGroupId_t | groupId, |
||
uint8_t * | groupName, |
||
uint8_t * | groupNameLength |
||
) |
This function gets a group name and its length.
- Parameters
-
endpointId
An endpoint identifier groupId
A group identifier groupName
An array pointer which will contain the group name groupNameLength
A pointer which will contain the group name length
- Returns
true
if group name was retrieved successfully,false
otherwise.
bool emberZclIsEndpointInGroup | ( | EmberZclEndpointId_t | endpointId, |
EmberZclGroupId_t | groupId |
||
) |
This function determines if an endpoint is a member of a group.
- Parameters
-
endpointId
An endpoint identifier groupId
A group identifier
- Returns
true
if the endpoint is a member of the group,false
otherwise.
EmberZclStatus_t emberZclRemoveAllGroups | ( | void |
| ) |
This function removes all groups.
- Returns
- EMBER_ZCL_STATUS_SUCCESS if all groups were removed (other than the all-endpoints group)
- EMBER_ZCL_STATUS_NOT_FOUND if no groups exist (other than the all-endpoints group)
EmberZclStatus_t emberZclRemoveEndpointFromAllGroups | ( | EmberZclEndpointId_t | endpointId | ) |
This function removes an endpoint from all groups to which it belongs.
- Parameters
-
endpointId
An endpoint identifier
- Returns
- EMBER_ZCL_STATUS_SUCCESS if the endpoint was removed from one or more groups
- EMBER_ZCL_STATUS_NOT_FOUND if the endpoint is not a member of any group (other than the all-endpoints group)
EmberZclStatus_t emberZclRemoveEndpointFromGroup | ( | EmberZclEndpointId_t | endpointId, |
EmberZclGroupId_t | groupId |
||
) |
This function removes an endpoint from a group.
- Parameters
-
endpointId
An endpoint identifier groupId
A group identifier
- Returns
- EMBER_ZCL_STATUS_SUCCESS if the endpoint was removed from the group
- EMBER_ZCL_STATUS_NOT_FOUND if the endpoint is not a member of the group
- EMBER_ZCL_STATUS_INVALID_FIELD if the groupId is not a value between EMBER_ZCL_GROUP_MIN and EMBER_ZCL_GROUP_MAX inclusive
EmberZclStatus_t emberZclRemoveGroup | ( | EmberZclGroupId_t | groupId | ) |
This function removes a group.
- Parameters
-
groupId
A group identifier
- Returns
- EMBER_ZCL_STATUS_SUCCESS if the group was removed
- EMBER_ZCL_STATUS_NOT_FOUND if the group does not exist
- EMBER_ZCL_STATUS_INVALID_FIELD if the groupId is not a value between EMBER_ZCL_GROUP_MIN and EMBER_ZCL_GROUP_MAX inclusive