Additional information about an incoming response.

#include <coap.h>

Data Fields

EmberIpv6Address localAddress
 
EmberIpv6Address remoteAddress
 
uint16_t localPort
 
uint16_t remotePort
 
void * applicationData
 
uint16_t applicationDataLength

Field Documentation

void* EmberCoapResponseInfo::applicationData

The value passed to emberCoapSend().

uint16_t EmberCoapResponseInfo::applicationDataLength

The value passed to emberCoapSend().

EmberIpv6Address EmberCoapResponseInfo::localAddress
uint16_t EmberCoapResponseInfo::localPort
EmberIpv6Address EmberCoapResponseInfo::remoteAddress
uint16_t EmberCoapResponseInfo::remotePort

The documentation for this struct was generated from the following file:
  • coap.h