EmberCoapOption Struct Reference
Structure that includes options in outgoing requests and responses.
#include <
coap.h
>
Data Fields | |
EmberCoapOptionType | type |
const uint8_t * | value |
uint16_t | valueLength |
uint32_t | intValue |
Calls that send messages can be passed a pointer to any array of EmberCoapOption
s.
Field Documentation
uint32_t EmberCoapOption::intValue |
The value of the option interpreted as a uint32_t.
EmberCoapOptionType EmberCoapOption::type |
The type of the option.
const uint8_t* EmberCoapOption::value |
A pointer to the option's value.
uint16_t EmberCoapOption::valueLength |
Number of bytes in the option's value.
The documentation for this struct was generated from the following file:
coap.h