EmberNetworkParameters Struct Reference
An application structure to hold useful network parameters.
#include <
network-management.h
>
Data Fields | |
uint8_t | networkId [EMBER_NETWORK_ID_SIZE] |
This will only be NUL terminated if the length of the network id is less than EMBER_NETWORK_ID_SIZE. | |
EmberIpv6Prefix | ulaPrefix |
uint8_t | extendedPanId [EXTENDED_PAN_ID_SIZE] |
uint16_t | panId |
uint8_t | channel |
EmberNodeType | nodeType |
int8_t | radioTxPower |
EmberKeyData | masterKey |
uint8_t | joinKey [EMBER_JOIN_KEY_MAX_SIZE] |
This will only be NUL terminated if the length of the key is less than EMBER_JOIN_KEY_MAX_SIZE. | |
uint8_t | joinKeyLength |
Field Documentation
uint8_t EmberNetworkParameters::channel |
uint8_t EmberNetworkParameters::extendedPanId[EXTENDED_PAN_ID_SIZE] |
uint8_t EmberNetworkParameters::joinKey[EMBER_JOIN_KEY_MAX_SIZE] |
uint8_t EmberNetworkParameters::joinKeyLength |
EmberKeyData EmberNetworkParameters::masterKey |
uint8_t EmberNetworkParameters::networkId[EMBER_NETWORK_ID_SIZE] |
EmberNodeType EmberNetworkParameters::nodeType |
uint16_t EmberNetworkParameters::panId |
int8_t EmberNetworkParameters::radioTxPower |
EmberIpv6Prefix EmberNetworkParameters::ulaPrefix |
The documentation for this struct was generated from the following file:
network-management.h