Color Control Server Callbacks
Functions | |
void | emberAfPluginColorControlServerComputePwmFromHsvCallback (uint8_t endpoint) |
Compute Pwm from HSV. | |
void | emberAfPluginColorControlServerComputePwmFromXyCallback (uint8_t endpoint) |
Compute Pwm from HSV. | |
void | emberAfPluginColorControlServerComputePwmFromTempCallback (uint8_t endpoint) |
Compute Pwm from HSV. |
Detailed Description
These callbacks are contributed by the Color Control Server plugin.
Function Documentation
void emberAfPluginColorControlServerComputePwmFromHsvCallback | ( | uint8_t | endpoint | ) |
This function is called from the color server when it is time for the PWMs to be driven with a new value from the HSV values.
- Parameters
-
endpoint
The identifying endpoint Ver.: always
void emberAfPluginColorControlServerComputePwmFromTempCallback | ( | uint8_t | endpoint | ) |
This function is called from the color server when it is time for the PWMs to be driven with a new value from the color temperature.
- Parameters
-
endpoint
The identifying endpoint Ver.: always
void emberAfPluginColorControlServerComputePwmFromXyCallback | ( | uint8_t | endpoint | ) |
This function is called from the color server when it is time for the PWMs to be driven with a new value from the color X and color Y values.
- Parameters
-
endpoint
The identifying endpoint Ver.: always