USB_Setup_TypeDef Struct Reference
USB Setup request package.
#include <
em_usb.h
>
Data Fields | |
union { | |
struct { | |
union { | |
struct { | |
uint8_t Recipient: 5 | |
uint8_t Type: 2 | |
uint8_t Direction: 1 | |
} | |
uint8_t bmRequestType | |
} | |
uint8_t bRequest | |
uint16_t wValue | |
uint16_t wIndex | |
uint16_t wLength | |
} | |
uint32_t dw [2] | |
}; |
Field Documentation
union { ... } |
uint8_t USB_Setup_TypeDef::bmRequestType |
Request characteristics.
uint8_t USB_Setup_TypeDef::bRequest |
Request code.
uint8_t USB_Setup_TypeDef::Direction |
Transfer direction of SETUP data phase.
uint32_t USB_Setup_TypeDef::dw[2] |
uint8_t USB_Setup_TypeDef::Recipient |
Request recipient (device, interface, endpoint or other).
uint8_t USB_Setup_TypeDef::Type |
Request type (standard, class or vendor).
uint16_t USB_Setup_TypeDef::wIndex |
Index or offset, varies according to request.
uint16_t USB_Setup_TypeDef::wLength |
Number of bytes to transfer if there is a data stage.
uint16_t USB_Setup_TypeDef::wValue |
Varies according to request.
The documentation for this struct was generated from the following file:
em_usb.h