Forming and Joining
Forming and Joining Utilities.
Macros |
|
#define | EMBER_USE_DEFAULTS 0 |
The following denotes which network parameters to use when forming or joining a network. Construct an uint16_t "options" flag for use in various network formation calls.
|
|
#define | EMBER_NETWORK_ID_OPTION BIT (0) |
#define | EMBER_ULA_PREFIX_OPTION BIT (1) |
#define | EMBER_EXTENDED_PAN_ID_OPTION BIT (2) |
#define | EMBER_PAN_ID_OPTION BIT (3) |
#define | EMBER_NODE_TYPE_OPTION BIT (4) |
#define | EMBER_TX_POWER_OPTION BIT (5) |
#define | EMBER_MASTER_KEY_OPTION BIT (6) |
#define | EMBER_JOIN_KEY_OPTION BIT (8) |
Functions |
|
void | emberConfigureNetwork (const EmberNetworkParameters *parameters, uint16_t options) |
This function configures network parameters.
|
|
void | emberFormNetwork (const EmberNetworkParameters *parameters, uint16_t options, uint32_t channelMask) |
This function forms a new network.
|
|
void | emberFormNetworkReturn ( EmberStatus status) |
A callback that indicates whether a prior call to
emberFormNetwork()
successfully initiated the form process. The status argument is either EMBER_SUCCSS, or EMBER_INVALID_CALL if resume was called when the network status was not EMBER_NO_NETWORK, or a scan was underway.
|
|
void | emberJoinNetwork (const EmberNetworkParameters *parameters, uint16_t options, uint32_t channelMask) |
This function joins an existing network.
|
|
void | emberJoinCommissioned (int8_t radioTxPower, EmberNodeType nodeType, bool requireConnectivity) |
This function joins an already-commissioned network.
|
|
void | emberJoinNetworkReturn ( EmberStatus status) |
A callback that indicates whether the join process was successfully initiated via a prior call to
emberJoinNetwork()
or
emberJoinCommissioned()
. The possible EmberStatus values are: EMBER_SUCCESS, EMBER_BAD_ARGUMENT, or EMBER_INVALID_CALL (if join was called when the network status was something other than EMBER_NO_NETWORK).
|
|
void | emberResumeNetwork (void) |
This function resumes network operation after a reboot of the Ember micro.
|
|
void | emberResumeNetworkReturn ( EmberStatus status) |
A callback that indicates whether a prior call to
emberResumeNetwork()
successfully initiated the resume process. The status argument is either EMBER_SUCCESS, or EMBER_INVALID_CALL if resume was called when the network status was not EMBER_SAVED_NETWORK, or while a scan was underway.
|
|
void | emberAttachToNetwork (void) |
On an end device, this initiates an attach with any available router-eligible devices in the network. This call must only be made if the network materials have been pre-commissioned on this device, or if previously completed obtaining the commissioning materials from another device.
|
|
void | emberAttachToNetworkReturn ( EmberStatus status) |
A callback that indicates whether the attach process was successfully initiated via a prior call to
emberAttachToNetwork()
. The status argument is either EMBER_SUCCESS, or EMBER_INVALID_CALL if attach was called when the network status was not EMBER_JOINED_NETWORK_NO_PARENT, or while an attach was underway.
|
|
void | emberSetAddressHandler (const uint8_t *address) |
A callback that is generated when the host's address changes.
|
|
void | emberSetDriverAddressHandler (const uint8_t *address) |
A callback to the IP driver to tell it to change its address.
|
|
void | emberStartHostJoinClientHandler (const uint8_t *parentAddress) |
A callback to tell the host to start security commissioning.
|
|
void | emberSetNetworkKeysHandler (uint32_t sequence, const uint8_t *masterKey, uint32_t sequence2, const uint8_t *masterKey2) |
A callback to the IP driver to tell it the network keys.
|
|
void | emberSetCommProxyAppParametersHandler (const uint8_t *extendedPanId, const uint8_t *networkId, const uint8_t *ulaPrefix, uint16_t panId, uint8_t channel, const EmberEui64 *eui64, const EmberEui64 *macExtendedId, EmberNetworkStatus networkStatus) |
A callback to provide the commission-proxy-app on the host with the requisite network parameters.
|
|
void | emberSetCommProxyAppSecurityHandler (const uint8_t *masterKey, uint32_t sequenceNumber) |
A callback to provide the commission-proxy-app on the host with the requisite security material.
|
|
void | emberSetCommProxyAppAddressHandler (const uint8_t *address) |
A callback to provide the commission-proxy-app on the host with our mesh local address.
|
|
void | emberSetCommProxyAppPskcHandler (const uint8_t *pskc) |
A callback to provide the commission-proxy-app on the host with the pskc.
|
|
void | emberChangeNodeType ( EmberNodeType newType) |
This function changes the node type of a joined device.
|
|
void | emberChangeNodeTypeReturn ( EmberStatus status) |
This function provides the result of a call to
emberChangeNodeType()
: either EMBER_SUCCESS, or EMBER_INVALID_CALL.
|
Detailed Description
See
network-management.h
for source code.
Macro Definition Documentation
#define EMBER_EXTENDED_PAN_ID_OPTION BIT (2) |
#define EMBER_JOIN_KEY_OPTION BIT (8) |
#define EMBER_MASTER_KEY_OPTION BIT (6) |
#define EMBER_NETWORK_ID_OPTION BIT (0) |
#define EMBER_NODE_TYPE_OPTION BIT (4) |
#define EMBER_PAN_ID_OPTION BIT (3) |
#define EMBER_TX_POWER_OPTION BIT (5) |
#define EMBER_ULA_PREFIX_OPTION BIT (1) |
#define EMBER_USE_DEFAULTS 0 |
Function Documentation
void emberAttachToNetwork | ( | void |
|
) |
The status of whether the attach process was initiated is reported to the application via emberAttachToNetworkReturn() . Changes to the network status resulting from the attach process are reported to the application via emberNetworkStatusHandler() .
This function may only be called when the network status is EMBER_JOINED_NETWORK_NO_PARENT and an attach is not already underway.
void emberAttachToNetworkReturn | ( | EmberStatus |
status
|
) |
void emberChangeNodeType | ( | EmberNodeType |
newType
|
) |
The device must be joined to a network prior to making this call.
- Parameters
-
newType
The node type to change to.
void emberChangeNodeTypeReturn | ( | EmberStatus |
status
|
) |
This function provides the result of a call to emberChangeNodeType() : either EMBER_SUCCESS, or EMBER_INVALID_CALL.
void emberConfigureNetwork | ( | const EmberNetworkParameters * |
parameters,
|
uint16_t |
options
|
||
) |
This function assigns the network configuration values that will be used when the device forms or joins a network.
This function may only be called when the network status is EMBER_NO_NETWORK. If the node was previously part of a network, use emberResumeNetwork() to recover after a reboot. To forget the network and return to a status of EMBER_NO_NETWORK, please read cautions for emberResetNetworkState() .
- Parameters
-
parameters
Some parameters may be supplied by the caller. options
A bitmask indicating which network parameters are being supplied by the caller. The following list enumerates the options that can be set.
- EMBER_NETWORK_ID_OPTION
- EMBER_EXTENDED_PAN_ID_OPTION
- EMBER_ULA_PREFIX_OPTION
- EMBER_MASTER_KEY_OPTION
- EMBER_PAN_ID_OPTION
void emberFormNetwork | ( | const EmberNetworkParameters * |
parameters,
|
uint16_t |
options,
|
||
uint32_t |
channelMask
|
||
) |
The forming node chooses a random extended pan ID, network ULA prefix, and pan ID for the new network. It peforms an energy scan of the channels indicated by the channelMask argument and selects the one with lowest detected energy. It performs an active scan on that channel to ensure there is no pan ID conflict. emberFormNetworkReturn() indicates whether the form process was initiated. Changes to the network status resulting from the form process are reported to the application via emberNetworkStatusHandler() .
This function may only be called when the network status is EMBER_NO_NETWORK, and when a scan is not underway. If the node was previously part of a network, use emberResumeNetwork() to recover after a reboot. To forget the network and return to a status of EMBER_NO_NETWORK, read cautions for emberResetNetworkState() .
- Parameters
-
parameters
Some parameters may be supplied by the caller. options
A bitmask indicating which network parameters are being supplied by the caller. The following list enumerates the allowed options and the default value used if the option is not specified: - EMBER_NETWORK_ID_OPTION default: ember
- EMBER_ULA_PREFIX_OPTION default: random
- EMBER_NODE_TYPE_OPTION default: EMBER_ROUTER
- EMBER_TX_POWER_OPTION default: 3
channelMask
A mask indicating the channels to be scanned. See emberStartScan() for format details.
void emberFormNetworkReturn | ( | EmberStatus |
status
|
) |
void emberJoinCommissioned | ( | int8_t |
radioTxPower,
|
EmberNodeType |
nodeType,
|
||
bool |
requireConnectivity
|
||
) |
This function assumes that commissioning data has already been cached via a call to emberConfigureNetwork() .
- Parameters
-
radioTxPower
Desired radio output power, in dBm. nodeType
Type of device. requireConnectivity
If commissioned join fails, specify whether this node should start a new fragment. Note: The short PAN ID MUST be commissioned if this is true.
void emberJoinNetwork | ( | const EmberNetworkParameters * |
parameters,
|
uint16_t |
options,
|
||
uint32_t |
channelMask
|
||
) |
The joining node performs an active scan of the channels indicated by the channelMask argument. It looks for networks matching the criteria specified via the supplied parameters, and which currently allow joining. The status of whether the join process was initiated is reported to the application via emberResumeNetworkReturn() . Changes to the network status resulting from the join process are reported to the application via emberNetworkStatusHandler() .
This function may only be called when the network status is EMBER_NO_NETWORK, and when a scan is not underway. If the node was previously part of a network, use emberResumeNetwork() to recover after a reboot. To forget the network and return to a status of EMBER_NO_NETWORK, please read cautions for emberResetNetworkState() .
- Parameters
-
parameters
Some parameters may be supplied by the caller. options
A bitmask indicating which network parameters are being supplied by the caller. The following list enumerates the allowed options and the default value used if the option is not specified: - EMBER_NETWORK_ID_OPTION default: looks for any network id
- EMBER_EXTENDED_PAN_ID_OPTION default: looks for any extended pan id
- EMBER_PAN_ID_OPTION default: looks for any pan id
- EMBER_NODE_TYPE_OPTION default: EMBER_ROUTER
- EMBER_TX_POWER_OPTION default: 3
- EMBER_JOIN_KEY_OPTION default: empty
channelMask
A mask indicating the channels to be scanned. See emberStartScan() for format details.
void emberJoinNetworkReturn | ( | EmberStatus |
status
|
) |
void emberResumeNetwork | ( | void |
|
) |
If the device was previously part of a network, it will recover its former network parameters including pan id, extended pan id, node type, etc. and resume participation in the network. The status of whether the resume process was initiated is reported to the application via emberResumeNetworkReturn() . Changes to the network status resulting from the resume process are reported to the application via emberNetworkStatusHandler() .
This function may only be called when the network status is EMBER_SAVED_NETWORK and when a scan is not underway.
void emberResumeNetworkReturn | ( | EmberStatus |
status
|
) |
void emberSetAddressHandler | ( | const uint8_t * |
address
|
) |
- Parameters
-
address
IP address, 16 bytes
A callback that is generated when the host's address changes.
- Parameters
-
address
IP address, 16 bytes
void emberSetCommProxyAppAddressHandler | ( | const uint8_t * |
address
|
) |
void emberSetCommProxyAppParametersHandler | ( | const uint8_t * |
extendedPanId,
|
const uint8_t * |
networkId,
|
||
const uint8_t * |
ulaPrefix,
|
||
uint16_t |
panId,
|
||
uint8_t |
channel,
|
||
const EmberEui64 * |
eui64,
|
||
const EmberEui64 * |
macExtendedId,
|
||
EmberNetworkStatus |
networkStatus
|
||
) |
void emberSetCommProxyAppPskcHandler | ( | const uint8_t * |
pskc
|
) |
void emberSetCommProxyAppSecurityHandler | ( | const uint8_t * |
masterKey,
|
uint32_t |
sequenceNumber
|
||
) |
void emberSetDriverAddressHandler | ( | const uint8_t * |
address
|
) |
- Parameters
-
address
IP address, 16 bytes
void emberSetNetworkKeysHandler | ( | uint32_t |
sequence,
|
const uint8_t * |
masterKey,
|
||
uint32_t |
sequence2,
|
||
const uint8_t * |
masterKey2
|
||
) |
- Parameters
-
sequence
sequence number masterKey
master key, 16 bytes sequence2
second sequence number masterKey2NotUsed
second key, 16 bytes
void emberStartHostJoinClientHandler | ( | const uint8_t * |
parentAddress
|
) |
- Parameters
-
address
parent IP address, 16 bytes
A callback to tell the host to start security commissioning.
- Parameters
-
address
parent IP address, 16 bytes