Structure that holds information about a routing table entry for use on the application. See
emberGetRipEntry
.
#include <
network-management.h
>
uint8_t EmberRipEntry::age
|
uint8_t EmberRipEntry::incomingLinkQuality
|
uint8_t EmberRipEntry::macExtendedId[8]
|
bool EmberRipEntry::mleSync
|
uint8_t EmberRipEntry::nextHopIndex
|
uint8_t EmberRipEntry::outgoingLinkQuality
|
uint8_t EmberRipEntry::ripMetric
|
int8_t EmberRipEntry::rollingRssi
|
uint8_t EmberRipEntry::routeDelta
|
The documentation for this struct was generated from the following file: