EmberZclGroupEntry_t Struct Reference
#include <
zcl-core-types.h
>
Data Fields | |
EmberZclGroupId_t | groupId |
EmberZclEndpointId_t | endpointId |
uint8_t | groupNameLength |
uint8_t | groupName [EMBER_ZCL_MAX_GROUP_NAME_LENGTH] |
This structure holds a group entry that represents membership of an endpoint in a group.
Field Documentation
EmberZclEndpointId_t EmberZclGroupEntry_t::endpointId |
An endpoint identifier of a group entry.
EmberZclGroupId_t EmberZclGroupEntry_t::groupId |
A group identifier of a group entry.
uint8_t EmberZclGroupEntry_t::groupName[EMBER_ZCL_MAX_GROUP_NAME_LENGTH] |
An array containing group name.
uint8_t EmberZclGroupEntry_t::groupNameLength |
Length of group name.
The documentation for this struct was generated from the following file:
zcl-core-types.h