Microphone Codec MSADPCM Callbacks
Functions | |
void | halMicrophoneCodecMsadpcmDataReadyCallback (uint8_t *data, uint8_t length) |
A callback called when new microphone data is ready. |
Detailed Description
These callbacks are contributed by the Microphone Codec MSADPCM plugin.
Function Documentation
void halMicrophoneCodecMsadpcmDataReadyCallback | ( | uint8_t * | data, |
uint8_t | length |
||
) |
This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.
- Parameters
-
data
Pointer to the data that is ready length
Length of the data