EmberCoapSendInfo Struct Reference
Optional information when sending a message.
#include <
coap.h
>
Data Fields | |
bool | nonConfirmed: 1 |
bool | multicastLoopback: 1 |
EmberIpv6Address | localAddress |
uint16_t | localPort |
uint16_t | remotePort |
const EmberCoapOption * | options |
uint8_t | numberOfOptions |
uint32_t | responseTimeoutMs |
const uint8_t * | responseAppData |
uint16_t | responseAppDataLength |
EmberCoapTransmitHandler | transmitHandler |
void * | transmitHandlerData |
For all fields a value of 0 or NULL means that the default will be used.
Multicast are always sent as unconfirmed.
Field Documentation
EmberIpv6Address EmberCoapSendInfo::localAddress |
Default is to let the IP stack choose
uint16_t EmberCoapSendInfo::localPort |
Defaults to the CoAP port (5683)
bool EmberCoapSendInfo::multicastLoopback |
Defaults to not looping back
bool EmberCoapSendInfo::nonConfirmed |
Defaults to confirmed
uint8_t EmberCoapSendInfo::numberOfOptions |
Defaults to zero
const EmberCoapOption* EmberCoapSendInfo::options |
Defaults to NULL
uint16_t EmberCoapSendInfo::remotePort |
Defaults to the CoAP port (5683)
const uint8_t* EmberCoapSendInfo::responseAppData |
Defaults to NULL
uint16_t EmberCoapSendInfo::responseAppDataLength |
Defaults to zero
uint32_t EmberCoapSendInfo::responseTimeoutMs |
Default is 'EMBER_COAP_DEFAULT_TIMEOUT_MS'
EmberCoapTransmitHandler EmberCoapSendInfo::transmitHandler |
Defaults to using UDP
void* EmberCoapSendInfo::transmitHandlerData |
Defaults to NULL
The documentation for this struct was generated from the following file:
coap.h