Time Client Callbacks
Functions | |
bool | emberZclClusterTimeClientTimeSyncCallback (EmberZclDestination_t *timeServer) |
Calls back user when a Network time server available. |
Detailed Description
These callbacks are contributed by the Time Client plugin.
Function Documentation
bool emberZclClusterTimeClientTimeSyncCallback | ( | EmberZclDestination_t * | timeServer | ) |
This function is called from the client when a Time Server is available on the network.
- Parameters
-
timeServer
Pointer to the destination of the Time Server Ver.: always
- Returns
- FALSE if the application is not handling the update of Time Servers on this node.
References FALSE.