EmberZclCommandContext_t Struct Reference
#include <
zcl-core-types.h
>
Data Fields | |
EmberIpv6Address | remoteAddress |
EmberCoapCode | code |
const EmberCoapRequestInfo * | info |
const uint8_t * | payload |
uint16_t | payloadLength |
EmberZclGroupId_t | groupId |
EmberZclEndpointId_t | endpointId |
const EmberZclClusterSpec_t * | clusterSpec |
EmberZclCommandId_t | commandId |
This structure holds a command context.
Field Documentation
const EmberZclClusterSpec_t* EmberZclCommandContext_t::clusterSpec |
A cluster specification of a command.
EmberCoapCode EmberZclCommandContext_t::code |
CoAP code of a command.
EmberZclCommandId_t EmberZclCommandContext_t::commandId |
A command identifier.
EmberZclEndpointId_t EmberZclCommandContext_t::endpointId |
An endpoint identifier of a command.
EmberZclGroupId_t EmberZclCommandContext_t::groupId |
A group identifier of a command.
const EmberCoapRequestInfo* EmberZclCommandContext_t::info |
EZ-Mode needs access to the request info structure
const uint8_t* EmberZclCommandContext_t::payload |
Payload of a command.
uint16_t EmberZclCommandContext_t::payloadLength |
Payload length of a command.
EmberIpv6Address EmberZclCommandContext_t::remoteAddress |
A remote address of a command.
The documentation for this struct was generated from the following file:
zcl-core-types.h