Thread Stack API Reference
Modules | |
Forming and Joining | |
Forming and Joining Utilities. | |
IPv6 | |
IPv6 Addressing Utilities. | |
Commissioning | |
Commissioning Utilities. | |
Network Utilities | |
Network Utilities. | |
Device Types | |
Device Types. | |
Utilities | |
General Utilities. | |
Messaging | |
Sending unicasts and multicasts. | |
Command Interpreter | |
The command interpreter. | |
Debugging Utilities | |
Debugging Utilities. | |
MFGLIB | |
Manufacturing Library. |
Detailed Description
The Silicon Labs Thread stack API reference guide is Doxygen-generated documentation that is rooted at THREAD HOME/documentation/Thread-Doxygen/index.html. This document contains a comprehensive list of APIs used to interface to the Thread network. These APIs concern network management, device and stack management (including management of stack tables, event scheduling, message buffers and security), messaging, fragmentation, serial communication, token access, peripheral access, bootload utilities, and so on.