Structure to hold information about an 802.15.4 beacon for use on the application.
#include <network-management.h
>
bool EmberMacBeaconData::allowingJoin |
uint8_t EmberMacBeaconData::channel |
uint8_t EmberMacBeaconData::extendedPanId[8] |
uint8_t EmberMacBeaconData::lqi |
uint8_t EmberMacBeaconData::macExtendedId[8] |
uint8_t EmberMacBeaconData::networkId[16] |
uint16_t EmberMacBeaconData::panId |
uint8_t EmberMacBeaconData::protocolId |
int8_t EmberMacBeaconData::rssi |
uint16_t EmberMacBeaconData::shortId |
uint8_t EmberMacBeaconData::steeringData[16] |
uint8_t EmberMacBeaconData::steeringDataLength |
uint8_t EmberMacBeaconData::version |
The documentation for this struct was generated from the following file: