Endpoints
Macros | |
#define | EMBER_ZCL_ENDPOINT_MIN 0x01 |
#define | EMBER_ZCL_ENDPOINT_MAX 0xF0 |
#define | EMBER_ZCL_ENDPOINT_NULL ((EmberZclEndpointId_t)-1) |
#define | EMBER_ZCL_ENDPOINT_INDEX_NULL ((EmberZclEndpointIndex_t)-1) |
#define | EMBER_ZCL_DEVICE_ID_NULL ((EmberZclDeviceId_t)-1) |
Typedefs | |
typedef uint8_t | EmberZclEndpointId_t |
typedef uint8_t | EmberZclEndpointIndex_t |
typedef uint16_t | EmberZclDeviceId_t |
Functions | |
EmberZclEndpointIndex_t | emberZclEndpointIdToIndex (EmberZclEndpointId_t endpointId, const EmberZclClusterSpec_t *clusterSpec) |
EmberZclEndpointId_t | emberZclEndpointIndexToId (EmberZclEndpointIndex_t index, const EmberZclClusterSpec_t *clusterSpec) |
Detailed Description
See zcl-core-types.h
for source code.
See zcl-core.h
for source code.
Macro Definition Documentation
#define EMBER_ZCL_DEVICE_ID_NULL ((EmberZclDeviceId_t)-1) |
A distinguished value that represents a null (invalid) device identifer.
#define EMBER_ZCL_ENDPOINT_INDEX_NULL ((EmberZclEndpointIndex_t)-1) |
A distinguished value that represents a null (invalid) endpoint index.
#define EMBER_ZCL_ENDPOINT_MAX 0xF0 |
A maximum endpoint identifer value.
#define EMBER_ZCL_ENDPOINT_MIN 0x01 |
A minimum endpoint identifer value.
#define EMBER_ZCL_ENDPOINT_NULL ((EmberZclEndpointId_t)-1) |
A distinguished value that represents a null (invalid) endpoint identifer.
Typedef Documentation
typedef uint16_t EmberZclDeviceId_t |
A device identifier.
typedef uint8_t EmberZclEndpointId_t |
An endpoint identifier.
typedef uint8_t EmberZclEndpointIndex_t |
An endpoint index.
Function Documentation
EmberZclEndpointIndex_t emberZclEndpointIdToIndex | ( | EmberZclEndpointId_t | endpointId, |
const EmberZclClusterSpec_t * | clusterSpec |
||
) |
This function finds the endpoint index for the specified endpoint identifier and cluster specification.
- Parameters
-
endpointId
An endpoint identifier clusterSpec
A cluster specification or NULL
- Returns
- An endpoint index or EMBER_ZCL_ENDPOINT_INDEX_NULL if no match is found.
This function searches the endpoint table and returns the endpoint index for the entry that matches the specified endpoint identifier and cluster specification. If clusterSpec is NULL, match on endpointId only.
- Note
- The endpoint index is the zero-based relative position of an endpoint among the subset of endpoints that support the specified cluster. For example, an index of 3 refers to the fourth endpoint that supports the specified cluster. The value of endpoint index for a given endpoint identifier may be different for different clusters.
- See also
- emberZclEndpointIndexToId()
EmberZclEndpointId_t emberZclEndpointIndexToId | ( | EmberZclEndpointIndex_t | index, |
const EmberZclClusterSpec_t * | clusterSpec |
||
) |
This function finds the endpoint identifier for the specified endpoint index and cluster specification.
- Parameters
-
index
An endpoint index clusterSpec
A cluster specification or NULL
- Returns
- An endpoint identifier or EMBER_ZCL_ENDPOINT_NULL if no match is found.
This function searches the endpoint table and returns the endpoint identifier for the entry that matches the specified endpoint index and cluster specification. If clusterSpec is NULL, match on index only.
- Note
- The endpoint index is the zero-based relative position of an endpoint among the subset of endpoints that support the specified cluster. For example, an index of 3 refers to the fourth endpoint that supports the specified cluster. The value of endpoint index for a given endpoint identifier may be different for different clusters.
- See also
- emberZclEndpointIdToIndex()