MacCountersData Struct Reference
#include <
network-diagnostics.h
>
Data Fields | |
uint16_t | packetsSent |
uint16_t | packetsReceived |
uint16_t | packetsDroppedOnTransmit |
uint16_t | packetsDroppedOnReceive |
uint16_t | securityErrors |
uint16_t | numberOfRetries |
Field Documentation
uint16_t MacCountersData::numberOfRetries |
uint16_t MacCountersData::packetsDroppedOnReceive |
uint16_t MacCountersData::packetsDroppedOnTransmit |
uint16_t MacCountersData::packetsReceived |
uint16_t MacCountersData::packetsSent |
uint16_t MacCountersData::securityErrors |
The documentation for this struct was generated from the following file:
network-diagnostics.h