Microphone IMAADPCM Callbacks

Functions

void halMicrophoneImaadpcmDataReadyCallback (uint8_t *data, uint8_t length)
 A callback called when new microphone data is ready.

Detailed Description

These callbacks are contributed by the Microphone IMAADPCM plugin.

Function Documentation

void halMicrophoneImaadpcmDataReadyCallback ( uint8_t *  data,
uint8_t  length 
)

This function is called by the plugin when new data has been processed and is ready to be processed by other parts of the system.

Parameters
dataPointer to the data that is ready
lengthLength of the data