Common bootloader interface defines and functions.

Macros

#define BOOTLOADER_BASE_TYPE (extendedType)   ((uint8_t)(((extendedType) >> 8U) & 0xFFU))
Macro returning the base type of a bootloader when given an extended type.
#define BOOTLOADER_MAKE_EXTENDED_TYPE (baseType, extendedSpecifier)   ((uint16_t)(((uint16_t)baseType) << 8U) | (((uint16_t)extendedSpecifier) & 0xFFU))
Macro returning the extended type of a bootloader when given a base type and extendedSpecifier.
#define BL_EXT_TYPE_NULL (( BL_TYPE_NULL << 8U) | 0x00U)
Macro defining the extended NULL bootloader type.
#define BL_EXT_TYPE_STANDALONE_UNKNOWN (( BL_TYPE_STANDALONE << 8U) | 0x00U)
Macro defining the extended standalone unknown bootloader type.
#define BL_EXT_TYPE_SERIAL_UART (( BL_TYPE_STANDALONE << 8U) | 0x01U)
Macro defining the extended standalone UART bootloader type.
#define BL_EXT_TYPE_SERIAL_UART_OTA (( BL_TYPE_STANDALONE << 8U) | 0x03U)
Macro defining the extended standalone OTA and UART bootloader type.
#define BL_EXT_TYPE_EZSP_SPI (( BL_TYPE_STANDALONE << 8U) | 0x04U)
#define BL_EXT_TYPE_EZSP_SPI_OTA (( BL_TYPE_STANDALONE << 8U) | 0x06U)
#define BL_EXT_TYPE_SERIAL_USB (( BL_TYPE_STANDALONE << 8U) | 0x07U)
Macro defining the extended standalone USB bootloader type.
#define BL_EXT_TYPE_SERIAL_USB_OTA (( BL_TYPE_STANDALONE << 8U) | 0x08U)
Macro defining the extended standalone OTA and USB bootloader type.
#define BL_EXT_TYPE_APP_UNKNOWN (( BL_TYPE_APPLICATION << 8U) | 0x00U)
Macro defining the extended application unknown bootloader type.
#define BL_EXT_TYPE_APP_SPI (( BL_TYPE_APPLICATION << 8U) | 0x01U)
Macro defining the extended application SPI bootloader type.
#define BL_EXT_TYPE_APP_I2C (( BL_TYPE_APPLICATION << 8U) | 0x02U)
Macro defining the extended application I2C bootloader type.
#define BL_EXT_TYPE_APP_LOCAL_STORAGE (( BL_TYPE_APPLICATION << 8U) | 0x03U)
Macro defining a type for the local storage app bootloader.
#define BOOTLOADER_INVALID_VERSION 0xFFFF
Define an invalid bootloader version.
#define CUSTOMER_APPLICATION_VERSION 0
Macro defining the customer application version stored in the ApplicationProperties_t struct.
#define CUSTOMER_APPLICATION_CAPABILITIES 0
Macro defining the customer application capabilities stored in the ApplicationProperties_t struct.
#define CUSTOMER_APPLICATION_PRODUCT_ID { 0 }
Macro defining the customer application product ID stored in the ApplicationProperties_t struct.
#define MPSI_PLUGIN_SUPPORT 0
Macro defining the support for the MPSI protocol stored in the capabilities field of the ApplicationProperties_t struct.
#define APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT 31
Macro defining the bit position that corresponds to MPSI support in the capabilities field of the ApplicationProperties_t struct.
#define APPLICATION_PROPERTIES_CAPABILITIES
Macro defining the capabilities that this application has. This value is set in the capabilities field of the ApplicationProperties_t struct.

Functions

BlBaseType halBootloaderGetType (void)
Returns the bootloader base type the application was built for.
BlExtendedType halBootloaderGetInstalledType (void)
Returns the extended bootloader type of the bootloader that is present on the chip.
uint16_t halGetBootloaderVersion (void)
Returns the version of the installed bootloader, regardless of its type.
void halGetExtendedBootloaderVersion (uint32_t *emberVersion, uint32_t *customerVersion)
Return extended bootloader version information, if supported. This API is not supported for EM2XX chips and only returns extra information on bootloaders built on or after the 4.7 release.

Bootloader Numerical Definitions

These are numerical definitions for the possible bootloader types and a typedef of the bootloader base type.

#define BL_TYPE_NULL (0)
Numerical definition for a bootloader type.
#define BL_TYPE_STANDALONE (1)
Numerical definition for a bootloader type.
#define BL_TYPE_APPLICATION (2)
Numerical definition for a bootloader type.
#define BL_TYPE_BOOTLOADER (3)
Numerical definition for a bootloader type.
#define BL_TYPE_SMALL_BOOTLOADER (4)
Numerical definition for a bootloader type.

Bootloader type definitions

These are the type definitions for the bootloader.

typedef uint8_t BlBaseType
Define the bootloader base type.
typedef uint16_t BlExtendedType
Define the bootloader extended type.

Detailed Description

See bootloader-interface.h for source code.

Macro Definition Documentation

#define APPLICATION_PROPERTIES_CAPABILITIES
Value:
#define APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT
Macro defining the bit position that corresponds to MPSI support in the capabilities field of the App...
Definition: bootloader-interface.h:195
#define MPSI_PLUGIN_SUPPORT
Macro defining the support for the MPSI protocol stored in the capabilities field of the ApplicationP...
Definition: bootloader-interface.h:189
#define CUSTOMER_APPLICATION_CAPABILITIES
Macro defining the customer application capabilities stored in the ApplicationProperties_t struct...
Definition: bootloader-interface.h:173
#define APPLICATION_PROPERTIES_CAPABILITIES_MPSI_SUPPORT_BIT   31
#define BL_EXT_TYPE_APP_I2C   (( BL_TYPE_APPLICATION << 8U) | 0x02U)
#define BL_EXT_TYPE_APP_LOCAL_STORAGE   (( BL_TYPE_APPLICATION << 8U) | 0x03U)
#define BL_EXT_TYPE_APP_SPI   (( BL_TYPE_APPLICATION << 8U) | 0x01U)
#define BL_EXT_TYPE_APP_UNKNOWN   (( BL_TYPE_APPLICATION << 8U) | 0x00U)
#define BL_EXT_TYPE_EZSP_SPI   (( BL_TYPE_STANDALONE << 8U) | 0x04U)
#define BL_EXT_TYPE_EZSP_SPI_OTA   (( BL_TYPE_STANDALONE << 8U) | 0x06U)
#define BL_EXT_TYPE_NULL   (( BL_TYPE_NULL << 8U) | 0x00U)
#define BL_EXT_TYPE_SERIAL_UART   (( BL_TYPE_STANDALONE << 8U) | 0x01U)
#define BL_EXT_TYPE_SERIAL_UART_OTA   (( BL_TYPE_STANDALONE << 8U) | 0x03U)
#define BL_EXT_TYPE_SERIAL_USB   (( BL_TYPE_STANDALONE << 8U) | 0x07U)
#define BL_EXT_TYPE_SERIAL_USB_OTA   (( BL_TYPE_STANDALONE << 8U) | 0x08U)
#define BL_EXT_TYPE_STANDALONE_UNKNOWN   (( BL_TYPE_STANDALONE << 8U) | 0x00U)
#define BL_TYPE_APPLICATION   (2)
#define BL_TYPE_BOOTLOADER   (3)
#define BL_TYPE_NULL   (0)
#define BL_TYPE_SMALL_BOOTLOADER   (4)
#define BL_TYPE_STANDALONE   (1)
#define BOOTLOADER_BASE_TYPE ( extendedType ) ((uint8_t)(((extendedType) >> 8U) & 0xFFU))
#define BOOTLOADER_INVALID_VERSION   0xFFFF
#define BOOTLOADER_MAKE_EXTENDED_TYPE ( baseType,
extendedSpecifier
) ((uint16_t)(((uint16_t)baseType) << 8U) | (((uint16_t)extendedSpecifier) & 0xFFU))
#define CUSTOMER_APPLICATION_CAPABILITIES   0
Note
The capabilities field in the ApplicationProperties_t struct is shared with other values.
#define CUSTOMER_APPLICATION_PRODUCT_ID   { 0 }
#define CUSTOMER_APPLICATION_VERSION   0
#define MPSI_PLUGIN_SUPPORT   0

Typedef Documentation

typedef uint8_t BlBaseType
typedef uint16_t BlExtendedType

Function Documentation

BlExtendedType halBootloaderGetInstalledType ( void )
uint16_t halGetBootloaderVersion ( void )
Returns
Version if bootloader installed, or BOOTLOADER_INVALID_VERSION . A returned version of 0x1234U would indicate version 1.2 build 34
void halGetExtendedBootloaderVersion ( uint32_t * emberVersion,
uint32_t * customerVersion
)
Parameters
emberVersion If specified, we will return the full 32bit ember version for this bootloader. Format is major, minor, patch, doc (4bit nibbles) followed by a 16bit build number.
customerVersion This will return the 32bit value specified in CUSTOMER_BOOTLOADER_VERSION at build time.