buffer-management API Callbacks
Functions | |
void * | emberAllocateMemoryForPacketHandler (uint32_t size, void **objectRef) |
This function can be used to hook an external memory allocator into the stack. It will be called when we need to allocate large packets. | |
void | emberFreeMemoryForPacketHandler (void *objectRef) |
This handler is called when freeing memory allocated with emberAllocateMemoryForPacketHandler. | |
void | emberMarkApplicationBuffersHandler (void) |
Applications that use buffers must mark them by defining this function. The stack uses this when reclaiming unused buffers. |
Detailed Description
These callbacks were contributed by the buffer-management API.
Function Documentation
void* emberAllocateMemoryForPacketHandler | ( | uint32_t | size, |
void ** | objectRef |
||
) |
If a value other than NULL is returned that pointer will be used to store packet data. You must also fill in the objectRef parameter with whatever reference you would like passed to the emberFreeMemoryForPacketHandler() when we're done with this memory. If you set the objectRef to NULL then the free handler will not be called.
- Parameters
-
size
size of packet data objectRef
Reference of the memory to be used in emberFreeMemoryForPacketHandler
- Returns
- pointer that stores the packet data
References NULL.
void emberFreeMemoryForPacketHandler | ( | void * | objectRef | ) |
- Parameters
-
objectRef
Reference used in emberAllocateMemoryForPacketHandler
void emberMarkApplicationBuffersHandler | ( | void |
| ) |