EmberSecurityParameters Struct Reference

Values of security parameters for use in forming or joining a network.

#include <network-management.h>

Data Fields

EmberKeyDatanetworkKey
 
uint8_t * presharedKey
 
uint8_t presharedKeyLength

Structure to hold information about pre-shared network security parameters.

Field Documentation

EmberKeyData* EmberSecurityParameters::networkKey
uint8_t* EmberSecurityParameters::presharedKey
uint8_t EmberSecurityParameters::presharedKeyLength

The documentation for this struct was generated from the following file:
  • network-management.h