connection-manager API Callbacks
Functions | |
void | emberConnectionManagerConnectCompleteCallback (EmberConnectionManagerConnectionStatus status) |
Connection attempt completed. |
Detailed Description
These callbacks were contributed by the connection-manager API.
Function Documentation
void emberConnectionManagerConnectCompleteCallback | ( | EmberConnectionManagerConnectionStatus | status | ) |
This function is called when an attempt to connect to a network has completed. It will convery the result of an attempt to join a network using the emberConnectionManagerStartConnect function. The status will be one of the following values:
EMBER_CONNECTION_MANAGER_STATUS_CONNECTED: The device succesfully attached to the network. EMBER_CONNECTION_MANAGER_STATUS_TIMED_OUT: The device was unable to join the network after attempting the number of times specified in the connection manager plugin options.