network-management API Callbacks
Functions | |
void | emberActiveScanHandler (const EmberMacBeaconData *beaconData) |
Reports an incoming beacon during an active scan. | |
void | emberAddressConfigurationChangeHandler (const EmberIpv6Address *address, uint32_t preferredLifetime, uint32_t validLifetime, uint8_t addressFlags) |
This is called when a new address is configured on the application. | |
void | emberAttachToNetworkReturn (EmberStatus status) |
A callback that indicates whether the attach process was successfully initiated via a prior call to emberAttachToNetwork(). The status argument is either EMBER_SUCCESS, or EMBER_INVALID_CALL if attach was called when the network status was not EMBER_JOINED_NETWORK_NO_PARENT, or while an attach was underway. | |
void | emberBecomeCommissionerReturn (EmberStatus status) |
Return call for emberBecomeCommissioner(). The status is EMBER_SUCCESS if a petition was sent or EMBER_ERR_FATAL if some temporary resource shortage prevented doing so. | |
void | emberChangeNodeTypeReturn (EmberStatus status) |
Provides the result of a call to emberChangeNodeType(): either EMBER_SUCCESS, or EMBER_INVALID_CALL. | |
void | emberAllowNativeCommissionerReturn (EmberStatus status) |
Provides the result of a call to emberAllowNativeCommissioner(): either EMBER_SUCCESS or EMBER_INVALID_CALL. | |
void | emberSetCommissionerKeyReturn (EmberStatus status) |
Provides the result of a call to emberSetCommissionerKey(): either EMBER_SUCCESS or EMBER_INVALID_CALL. | |
void | emberSetPskcHandler (const uint8_t *pskc) |
Handler to let application know that a PSKc TLV was successfully set. | |
void | emberSetJoinKeyReturn (EmberStatus status) |
Provides the result of a call to emberSetJoinKey(): either EMBER_SUCCESS or EMBER_BAD_ARGUMENT. | |
void | emberCommissionNetworkReturn (EmberStatus status) |
Provides the result of a call to emberCommissionNetwork. | |
void | emberCommissionerStatusHandler (uint16_t flags, const uint8_t *commissionerName, uint8_t commissionerNameLength) |
Reports on the current commissioner state. | |
void | emberConfigureGatewayReturn (EmberStatus status) |
Provides the result of a call to emberConfigureGateway. | |
void | emberSetNdDataReturn (EmberStatus status, uint16_t length) |
Provides the result of a call to emberSetNdData. | |
void | emberSetLocalNetworkDataReturn (EmberStatus status, uint16_t length) |
Provides the result of a call to emberSetLocalNetworkData. | |
void | emberConfigureExternalRouteReturn (EmberStatus status) |
Provides the result of a call to emberConfigureExternalRoute. | |
void | emberCounterHandler (EmberCounterType type, uint16_t increment) |
A callback invoked to inform the application of the occurrence of an event defined by EmberCounterType, for example, transmissions and receptions at different layers of the stack. | |
uint16_t | emberCounterValueHandler (EmberCounterType type) |
A callback invoked to query the application for the countervalue of an event defined by EmberCounterType. | |
void | emberResetCounterHandler (EmberCounterType type) |
A callback invoked to the application to reset the countervalue of an event defined by EmberCounterType. | |
void | emberCustomHostToNcpMessageHandler (const uint8_t *message, uint16_t messageLength) |
NCP handler called to process a custom message from the Host. | |
void | emberCustomNcpToHostMessageHandler (const uint8_t *message, uint16_t messageLength) |
Host handler called to process a custom message from the NCP. | |
void | emberDhcpServerChangeHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
This is called when the stack knows about a new dhcp server or if a dhcp server has become unavailable. | |
void | emberEnergyScanHandler (uint8_t channel, int8_t maxRssiValue) |
Reports the maximum RSSI value measured on the channel. | |
void | emberEventDelayUpdatedFromIsrHandler (Event *event) |
This method is called any time an event is scheduled from within an ISR context. It can be used to determine when to stop a long running sleep to see what application or stack events now need to be processed. | |
void | emberExternalRouteChangeHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
This is called when the stack knows about a border router that has an external route to a prefix. | |
void | emberFormNetworkReturn (EmberStatus status) |
A callback that indicates whether a prior call to emberFormNetwork() successfully initiated the form process. The status argument is either EMBER_SUCCSS, or EMBER_INVALID_CALL if resume was called when the network status was not EMBER_NO_NETWORK, or a scan was underway. | |
void | emberGetAntennaModeReturn (EmberStatus status, uint8_t mode) |
Provides the result of a call to emberGetAntennaMode . | |
void | emberGetCcaThresholdReturn (int8_t threshold) |
Provides the result of a call to emberGetCcaThreshold(). | |
void | emberGetChannelCalDataTokenReturn (uint8_t lna, int8_t tempAtLna, uint8_t modDac, int8_t tempAtModDac) |
Gets the token information for tokenId = EMBER_CHANNEL_CAL_DATA_TOKEN. | |
void | emberGetChildEntryReturn (uint8_t status, uint8_t index, uint8_t childTableSize, const EmberChildEntry *entry, const EmberIpv6Address *addresses, uint8_t addressCount) |
This callback returns the results of a call to emberGetChildEntry(). A status of EMBER_GET_CHILD_ENTRY_SUCCESS indicates a valid entry is being returned in the EmberChildEntry argument, located at the supplied index in the child table of size childTableSize. Note that the index returned is the smallest index not less than the index that was supplied to emberGetChildEntry(), which contains a valid child entry. | |
void | emberGetCounterReturn (EmberCounterType type, uint16_t value) |
Provides the result of a call to emberGetCounter(). | |
void | emberGetCtuneReturn (uint16_t tune, EmberStatus status) |
Provides the result of a call to emberGetCtune. | |
void | emberGetGlobalAddressReturn (const EmberIpv6Address *address, uint32_t preferredLifetime, uint32_t validLifetime, uint8_t addressFlags) |
Provides the result of a call to emberGetGlobalAddresses. | |
void | emberGetGlobalPrefixReturn (uint8_t flags, bool isStable, const uint8_t *prefix, uint8_t prefixLengthInBits, uint8_t domainId, uint32_t preferredLifetime, uint32_t validLifetime) |
Provides the result of a call to ::emberGetGlobalPrefix. | |
void | emberGetMfgTokenReturn (EmberMfgTokenId tokenId, EmberStatus status, const uint8_t *tokenData, uint8_t tokenDataLength) |
Provides the result of a call to emberGetMfgToken. | |
void | emberGetNetworkDataReturn (EmberStatus status, uint8_t *networkData, uint16_t bufferLength) |
Provides the result of a call to emberGetNetworkData. | |
void | emberGetNetworkDataTlvReturn (uint8_t typeByte, uint8_t index, uint8_t versionNumber, const uint8_t *tlv, uint8_t tlvLength) |
Provides the result of a call to emberGetNetworkDataTlv() . | |
void | emberGetPtaEnableReturn (bool enabled) |
Provides the result of a call to emberGetPtaEnable . | |
void | emberGetPtaOptionsReturn (uint32_t options) |
Provides the result of a call to emberGetPtaOptions . | |
void | emberGetPtaPwmOptionsReturn (uint8_t request, uint8_t dutyCycle, uint8_t periodHalfMs) |
This function provides the result of a call to emberGetPtaPwmOptions . | |
void | emberGetRadioPowerReturn (int8_t power) |
Provides the result of a call to emberGetRadioPower() on the host. | |
void | emberGetRipEntryReturn (uint8_t index, const EmberRipEntry *entry) |
Provides the result of a call to emberGetRipEntry(). | |
void | emberGetRoutingLocatorReturn (const EmberIpv6Address *rloc) |
Provides the result of a call to emberGetRoutingLocator. | |
void | emberGetStandaloneBootloaderInfoReturn (uint16_t version, uint8_t platformId, uint8_t microId, uint8_t phyId) |
Provides the result of a call to emberGetStandaloneBootloaderInfo. | |
void | emberGetTxPowerModeReturn (uint16_t txPowerMode) |
Provides the result of a call to emberGetTxPowerMode() on the host. | |
void | emberGetVersionsReturn (const uint8_t *versionName, uint16_t managementVersionNumber, uint16_t stackVersionNumber, uint16_t stackBuildNumber, EmberVersionType versionType, const uint8_t *buildTimestamp) |
Provides the result of a call to emberGetVersions(). | |
void | emberSetAddressHandler (const uint8_t *address) |
In a host/NCP setup, notifies the host to set the new mesh local address. | |
void | emberHostStateHandler (const EmberNetworkParameters *parameters, const EmberEui64 *localEui64, const EmberEui64 *macExtendedId, EmberNetworkStatus networkStatus) |
In a host/NCP setup, notifies the host to changes in the network parameters. | |
void | emberInitReturn (EmberStatus status) |
Provides the result of a call to emberInit(). | |
void | emberJoinNetworkReturn (EmberStatus status) |
A callback that indicates whether the join process was successfully initiated via a prior call to emberJoinNetwork() or emberJoinCommissioned(). The possible EmberStatus values are: EMBER_SUCCESS, EMBER_BAD_ARGUMENT, or EMBER_INVALID_CALL (if join was called when the network status was something other than EMBER_NO_NETWORK). | |
void | emberLaunchStandaloneBootloaderReturn (EmberStatus status) |
Provides the result of a call to emberLaunchStandaloneBootloader. | |
void | emberLeaderDataHandler (const uint8_t *leaderData) |
A callback invoked when the leader data changes. | |
bool | emberMacPassthroughFilterHandler (uint8_t *macHeader) |
Application handler to define "passthrough" packets. | |
void | emberMacPassthroughMessageHandler (PacketHeader header) |
Application handler to intercept "passthrough" packets and handle them at the application. | |
bool | emberMacRssiFilterHandler (uint8_t *macHeader) |
Application handler to filter 802.15.4 packets to be observed for signal strength. | |
void | emberMacRssiHandler (int8_t currentRssi) |
Gets the received signal strength indication (RSSI) for the last 802.15.4 packet received by the stack. | |
void | emberNetworkDataChangeHandler (const uint8_t *networkData, uint16_t length) |
This is called when the stack receives new Thread Network Data. | |
void | emberNetworkStatusHandler (EmberNetworkStatus newNetworkStatus, EmberNetworkStatus oldNetworkStatus, EmberJoinFailureReason reason) |
Reports a change to the network status. For example, the network status changes while going through the joining process, or while reattaching to the network, which can happen for a variety of reasons. In particular, after issuing a form, join, resume, or attach command, the application knows that the device is on the network and ready to communicate when this handler is called with a newNetworkStatus of EMBER_JOINED_NETWORK_ATTACHED. | |
void | emberOkToNapReturn (uint8_t stateMask) |
If implementing event-driven sleep on an NCP host, this method will return the bitmask indicating the stack's current tasks. (see enum above) | |
void | emberPollForDataReturn (EmberStatus status) |
Provides the result of a call to emberPollForData(). | |
void | emberRadioGetRandomNumbersReturn (EmberStatus status, const uint16_t *rn, uint8_t count) |
Provides the result of a call to emberRadioGetRandomNumbers . | |
void | emberRequestDhcpAddressReturn (EmberStatus status, const uint8_t *prefix, uint8_t prefixLengthInBits) |
Provides the result of a call to emberRequestDhcpAddress. | |
void | emberRequestSlaacAddressReturn (EmberStatus status, const uint8_t *prefix, uint8_t prefixLengthInBits) |
Provides the result of a call to emberRequestSlaacAddress. | |
void | emberResetMicroHandler (EmberResetCause cause) |
Notifies the application of a reset on the Ember chip due to the indicated cause. | |
void | emberResetNetworkStateReturn (EmberStatus status) |
Provides the result of a call to emberResetNetworkState(). | |
void | emberResignGlobalAddressReturn (EmberStatus status) |
Provides the result of a call to emberResignGlobalAddress(). | |
void | emberResumeNetworkReturn (EmberStatus status) |
A callback that indicates whether a prior call to emberResumeNetwork() successfully initiated the resume process. The status argument is either EMBER_SUCCESS, or EMBER_INVALID_CALL if resume was called when the network status was not EMBER_SAVED_NETWORK, or while a scan was underway. | |
void | emberScanReturn (EmberStatus status) |
Provides the status upon completion of a scan. | |
void | emberSendSteeringDataReturn (EmberStatus status) |
Provides the result of a call to emberSendSteeringData(). | |
void | emberSetAntennaModeReturn (EmberStatus status) |
Provides the result of a call to emberSetAntennaMode . | |
void | emberSetCcaThresholdReturn (EmberStatus status) |
Provides the result of a call to emberSetCcaThreshold(). | |
void | emberSetCtuneReturn (EmberStatus status) |
Provides the result of a call to emberSetCtune. | |
void | emberSetMfgTokenReturn (EmberMfgTokenId tokenId, EmberStatus status) |
Provides the result of a call to emberSetMfgToken. | |
void | emberSetPtaEnableReturn (EmberStatus status) |
Provides the result of a call to emberSetPtaEnable . | |
void | emberSetPtaOptionsReturn (EmberStatus status) |
Provides the result of a call to emberSetPtaOptions . | |
void | emberSetPtaPwmOptionsReturn (EmberStatus status) |
This function provides the result of a call to emberSetPtaPwmOptions . | |
void | emberSetRadioHoldOffReturn (EmberStatus status) |
Provides the result of a call to emberSetRadioHoldOff . | |
void | emberSetRadioPowerReturn (EmberStatus status) |
Provides the result of a call to emberSetRadioPower() on the host. | |
void | emberSetSecurityParametersReturn (EmberStatus status) |
Provides the result of a call to emberSetSecurityParameters(). | |
void | emberSetTxPowerModeReturn (EmberStatus status) |
Provides the result of a call to emberSetTxPowerMode() on the host. | |
void | emberSlaacServerChangeHandler (const uint8_t *prefix, uint8_t prefixLengthInBits, bool available) |
This is called when the stack knows about a new SLAAC prefix or if a SLAAC server has become unavailable. | |
void | emberStackPollForDataReturn (EmberStatus status) |
Provides the result of a call to emberStackPollForData(). | |
void | emberStartHostJoinClientHandler (const uint8_t *parentAddress) |
Callback to tell the host to start security commissioning. | |
void | emberStateReturn (const EmberNetworkParameters *parameters, const EmberEui64 *localEui64, const EmberEui64 *macExtendedId, EmberNetworkStatus networkStatus) |
In a host/NCP setup, provides the result of a call to emberState() on the host. | |
void | emberSwitchToNextNetworkKeyHandler (EmberStatus status) |
This can be stubbed out on the SoC and host app. It is used by the NCP to update security on the driver when it is instructed to switch the network key by an over the air update. | |
void | emberSwitchToNextNetworkKeyReturn (EmberStatus status) |
Provides the result of a call to emberSwitchToNextNetworkKey(). | |
void | emberSetDtlsDeviceCertificateReturn (uint32_t result) |
Provides the result of a call to emberSetDtlsDeviceCertificate(). | |
void | emberSetDtlsPresharedKeyReturn (EmberStatus status) |
Provides the result of a call to emberSetDtlsPresharedKey(). | |
void | emberOpenDtlsConnectionReturn (uint32_t result, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
Provides the result of a call to emberOpenDtlsConnection(). | |
void | emberDtlsSecureSessionEstablished (uint8_t flags, uint8_t sessionId, const EmberIpv6Address *localAddress, const EmberIpv6Address *remoteAddress, uint16_t localPort, uint16_t remotePort) |
Indicates to the application that a secure connection was successfully established. | |
void | emberCloseDtlsConnectionReturn (uint8_t sessionId, EmberStatus status) |
Provides the result of a call to emberCloseDtlsConnection(), or indicates that the connection was closed on the other end. | |
void | emberProcessCoap (const uint8_t *message, uint16_t messageLength, EmberCoapRequestInfo *info) |
Process a CoAP message received over an alternate transport. | |
void | emberMicroBusyHandler (bool busy) |
Callback informing the application running on the micro of interruptions to normal processing. If ::busy is true, the micro will be busy processing and unavailable for an indefinite period of time. If ::busy is false, the micro has resumed normal operation. The main use case is jpake crypto on EM3xx processors. This gives the application a chance to prepare for the pause in regular processing. |
Detailed Description
These callbacks were contributed by the network-management API.
Function Documentation
void emberActiveScanHandler | ( | const EmberMacBeaconData * | beaconData | ) |
This function reports an incoming beacon during an active scan.
void emberAddressConfigurationChangeHandler | ( | const EmberIpv6Address * | address, |
uint32_t | preferredLifetime, |
||
uint32_t | validLifetime, |
||
uint8_t | addressFlags |
||
) |
This function is called when a new address is configured on the application.
If addressFlags is EMBER_LOCAL_ADDRESS, it means that the address configured is a Thread-local address.
Otherwise, it means that the address assigned is a global address (DHCP or SLAAC).
In either case, if the valid lifetime is zero, then the address is no longer available.
- Parameters
-
address
the address preferredLifetime
the preferred lifetime of the address (in seconds) validLifetime
the valid lifetime of the address (in seconds) addressFlags
address configuration flags (see LocalServerFlag_e)
void emberAllowNativeCommissionerReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberAllowNativeCommissioner(): either EMBER_SUCCESS or EMBER_INVALID_CALL.
void emberAttachToNetworkReturn | ( | EmberStatus | status | ) |
void emberBecomeCommissionerReturn | ( | EmberStatus | status | ) |
void emberChangeNodeTypeReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberChangeNodeType(): either EMBER_SUCCESS, or EMBER_INVALID_CALL.
void emberCloseDtlsConnectionReturn | ( | uint8_t | sessionId, |
EmberStatus | status |
||
) |
- Parameters
-
sessionId
sessionId used for secure CoAP transport. status
- EMBER_SUCCESS - Successfully closed the connection
- EMBER_INVALID_CALL - Invalid session ID
- EMBER_ERR_FATAL - Fatal error closing the connection
void emberCommissionerStatusHandler | ( | uint16_t | flags, |
const uint8_t * | commissionerName, |
||
uint8_t | commissionerNameLength |
||
) |
This function reports on the current commissioner state.
- Parameters
-
flags
A combination of zero or more of the following: - EMBER_HAVE_COMMISSIONER a commissioner is active in the network
- EMBER_AM_COMMISSIONER this device is the active commissioner if emberStopCommissioning is called, then this flag is not returned as we are open to commissioner petitions
- EMBER_JOINING_ENABLED joining is enabled
- EMBER_JOINING_WITH_EUI_STEERING steering data restricts which devices can join. if not set, no restriction, any device can join (significant only when EMBER_JOINING_ENABLED is set)
commissionerName
The name of the active commissioner, or NULL if there is none or the name is not known. commissionerNameLength
The length of commissonerName.
void emberCommissionNetworkReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberCommissionNetwork.
Returns EMBER_SUCCESS if successful EMBER_BAD_ARGUMENT if any of the options are wrong EMBER_INVALID_CALL if the node is already on a network
- Parameters
-
status
Whether the call to emberCommissionNetwork was successful
void emberConfigureExternalRouteReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberConfigureExternalRoute.
void emberConfigureGatewayReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberConfigureGateway.
void emberCounterHandler | ( | EmberCounterType | type, |
uint16_t | increment |
||
) |
The application must define EMBER_APPLICATION_HAS_COUNTER_HANDLER in its CONFIGURATION_HEADER to use this. This function may be called in ISR context, so processing should be kept to a minimum.
- Parameters
-
type
The type of the event. increment
Specify the increase in the counter's tally.
uint16_t emberCounterValueHandler | ( | EmberCounterType | type | ) |
The application must define EMBER_APPLICATION_HAS_COUNTER_VALUE_HANDLER in its CONFIGURATION_HEADER to use this.
- Parameters
-
type
The type of the event.
- Returns
- The counter's tally.
void emberCustomHostToNcpMessageHandler | ( | const uint8_t * | message, |
uint16_t | messageLength |
||
) |
- Parameters
-
message
message received messageLength
length of message
void emberCustomNcpToHostMessageHandler | ( | const uint8_t * | message, |
uint16_t | messageLength |
||
) |
- Parameters
-
message
message received messageLength
length of message
void emberDhcpServerChangeHandler | ( | const uint8_t * | prefix, |
uint8_t | prefixLengthInBits, |
||
bool | available |
||
) |
This function is called when the stack knows about a new dhcp server or if a dhcp server has become unavailable.
"available" means the DHCP server can offer us an address if requested.
- Parameters
-
prefix
dhcp server prefix prefixLengthInBits
length in bits of the prefix available
whether this dhcp server is available
void emberDtlsSecureSessionEstablished | ( | uint8_t | flags, |
uint8_t | sessionId, |
||
const EmberIpv6Address * | localAddress, |
||
const EmberIpv6Address * | remoteAddress, |
||
uint16_t | localPort, |
||
uint16_t | remotePort |
||
) |
- Parameters
-
flags
1 = server, 0 = client (possibly other info later) sessionId
sessionId used for secure CoAP transport localAddress
local IPv6 address remoteAddress
remote IPv6 address localPort
local port remotePort
remote port
void emberEnergyScanHandler | ( | uint8_t | channel, |
int8_t | maxRssiValue |
||
) |
This function reports the maximum RSSI value measured on the channel.
- Parameters
-
channel
The 802.15.4 channel on which the RSSI value was measured. maxRssiValue
The maximum RSSI value measured (in units of dBm).
void emberEventDelayUpdatedFromIsrHandler | ( | Event * | event | ) |
- Parameters
-
event
The event that was scheduled by the ISR.
void emberExternalRouteChangeHandler | ( | const uint8_t * | prefix, |
uint8_t | prefixLengthInBits, |
||
bool | available |
||
) |
This function is called when the stack knows about a border router that has an external route to a prefix.
- Parameters
-
prefix
external route prefix prefixLengthInBits
length in bits of the prefix available
whether this external route is available.
void emberFormNetworkReturn | ( | EmberStatus | status | ) |
void emberGetAntennaModeReturn | ( | EmberStatus | status, |
uint8_t | mode |
||
) |
This function provides the result of a call to emberGetAntennaMode
.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure. mode
the current antenna mode, 0-primary, 1-secondary, 2-toggle on tx ack fail
void emberGetCcaThresholdReturn | ( | int8_t | threshold | ) |
This function provides the result of a call to emberGetCcaThreshold().
void emberGetChannelCalDataTokenReturn | ( | uint8_t | lna, |
int8_t | tempAtLna, |
||
uint8_t | modDac, |
||
int8_t | tempAtModDac |
||
) |
This function gets the token information for tokenId = EMBER_CHANNEL_CAL_DATA_TOKEN.
- Parameters
-
lna
[msb: cal needed? | bit 0-5: lna tune value] tempAtLna
[the temp (degC) when the LNA was calibrated] #param modDac [msb: cal needed? | bit 0-5: modulation DAC tune value] tempAtModDac
[the temp (degC) when the mod DAC was calibrated]
void emberGetChildEntryReturn | ( | uint8_t | status, |
uint8_t | index, |
||
uint8_t | childTableSize, |
||
const EmberChildEntry * | entry, |
||
const EmberIpv6Address * | addresses, |
||
uint8_t | addressCount |
||
) |
If the child is not a Full Thread Device (as indicated in the EmberChildEntry flags field), the parent stores the child's ipv6 addresses, which are then returned by this callback as well.
A status of EMBER_GET_CHILD_ENTRY_FAILURE indicates that no valid child entry was found at or above the requested index.
void emberGetCounterReturn | ( | EmberCounterType | type, |
uint16_t | value |
||
) |
This function provides the result of a call to emberGetCounter().
void emberGetCtuneReturn | ( | uint16_t | tune, |
EmberStatus | status |
||
) |
This function provides the result of a call to emberGetCtune.
- Parameters
-
tune
The current CTUNE value. status
An EmberStatus value indicating success or the reason for failure.
void emberGetGlobalAddressReturn | ( | const EmberIpv6Address * | address, |
uint32_t | preferredLifetime, |
||
uint32_t | validLifetime, |
||
uint8_t | addressFlags |
||
) |
This function provides the result of a call to emberGetGlobalAddresses.
- Parameters
-
address
IPv6 global address preferredLifetime
Preferred lifetime (in seconds) validLifetime
Valid lifetime (in seconds) addressFlags
Address configuration flags (EMBER_GLOBAL_ADDRESS_*)
void emberGetGlobalPrefixReturn | ( | uint8_t | flags, |
bool | isStable, |
||
const uint8_t * | prefix, |
||
uint8_t | prefixLengthInBits, |
||
uint8_t | domainId, |
||
uint32_t | preferredLifetime, |
||
uint32_t | validLifetime |
||
) |
This function provides the result of a call to ::emberGetGlobalPrefix.
- Parameters
-
flags
Please ignore this param, it is currently unused. (returns 0) isStable
Stable or temporary prefix prefix
Border router prefix prefixLengthInBits
Prefix length in bits domainId
Provisioning domain ID preferredLifetime
Preferred lifetime (in seconds) validLifetime
Valid lifetime (in seconds)
void emberGetMfgTokenReturn | ( | EmberMfgTokenId | tokenId, |
EmberStatus | status, |
||
const uint8_t * | tokenData, |
||
uint8_t | tokenDataLength |
||
) |
This function provides the result of a call to emberGetMfgToken.
- Parameters
-
tokenId
Which manufacturing token read. status
An EmberStatus value indicating success or the tokenData
The manufacturing token data. tokenDataLength
The length of the tokenData parameter in bytes.
void emberGetNetworkDataReturn | ( | EmberStatus | status, |
uint8_t * | networkData, |
||
uint16_t | bufferLength |
||
) |
This function provides the result of a call to emberGetNetworkData.
The status value is one of:
- EMBER_SUCCESS
- EMBER_NETWORK_DOWN
- EMBER_BAD_ARGUMENT (the supplied buffer was too small)
- Parameters
-
status
networkData
location of the Network Data dataLength
length in bytes of the Network Data
void emberGetNetworkDataTlvReturn | ( | uint8_t | typeByte, |
uint8_t | index, |
||
uint8_t | versionNumber, |
||
const uint8_t * | tlv, |
||
uint8_t | tlvLength |
||
) |
This function provides the result of a call to emberGetNetworkDataTlv()
.
- Parameters
-
type
the type of TLV returned. This is the same value as the value specified in the emberGetNetworkDataTlv()
call.index
the instance number of the TLV. This is the same value as the value specified in the emberGetNetworkDataTlv()
call.versionNumber
the network data version tlv
the TLV corresponding to type or NULL. tlvLength
length of tlv
void emberGetPtaEnableReturn | ( | bool | enabled | ) |
This function provides the result of a call to emberGetPtaEnable
.
- Parameters
-
enabled
When true, indicates packet traffic arbitration is enabed. When false, indicates packet traffic arbitration is disabled.
void emberGetPtaOptionsReturn | ( | uint32_t | options | ) |
This function provides the result of a call to emberGetPtaOptions
.
- Parameters
-
indicates
packet traffic arbitration options bit field. Field Bit Position Size(bits) RX retry timeout ms 0 8 Enable ack radio holdoff 8 1 Abort mid TX if grant is lost 9 1 TX request is high priority 10 1 RX request is high prioirity 11 1 RX retry request is high priority 12 1 RX retry request is enabled 13 1 Radio holdoff is enabled 14 1 Toggle request on mac retransmit 15 1 Reserved 16 15 Hold request across CCA failures 31 1
void emberGetPtaPwmOptionsReturn | ( | uint8_t | request, |
uint8_t | dutyCycle, |
||
uint8_t | periodHalfMs |
||
) |
- Parameters
-
request
PTA PWM bit field Field Bit Position Size(bits) Request enabled 0 1 Priority enabled 1 1 dutyCycle
PTA PWM duty cycle percentage(0-100) periodHalfMs
PTA PWM request period in half milliseconds
void emberGetRadioPowerReturn | ( | int8_t | power | ) |
This function provides the result of a call to emberGetRadioPower() on the host.
void emberGetRipEntryReturn | ( | uint8_t | index, |
const EmberRipEntry * | entry |
||
) |
This function provides the result of a call to emberGetRipEntry().
void emberGetRoutingLocatorReturn | ( | const EmberIpv6Address * | rloc | ) |
This function provides the result of a call to emberGetRoutingLocator.
- Parameters
-
rloc
The Routing Locator as a full IPv6 address.
void emberGetStandaloneBootloaderInfoReturn | ( | uint16_t | version, |
uint8_t | platformId, |
||
uint8_t | microId, |
||
uint8_t | phyId |
||
) |
This function provides the result of a call to emberGetStandaloneBootloaderInfo.
- Parameters
-
version
BOOTLOADER_INVALID_VERSION if the standalone bootloader is not present, or the version of the installed standalone bootloader. platformId
The value of PLAT on the node. microId
The value of MICRO on the node. phyId
The value of PHY on the node.
void emberGetTxPowerModeReturn | ( | uint16_t | txPowerMode | ) |
This function provides the result of a call to emberGetTxPowerMode() on the host.
- Returns
- the current tx power mode.
void emberGetVersionsReturn | ( | const uint8_t * | versionName, |
uint16_t | managementVersionNumber, |
||
uint16_t | stackVersionNumber, |
||
uint16_t | stackBuildNumber, |
||
EmberVersionType | versionType, |
||
const uint8_t * | buildTimestamp |
||
) |
void emberHostStateHandler | ( | const EmberNetworkParameters * | parameters, |
const EmberEui64 * | localEui64, |
||
const EmberEui64 * | macExtendedId, |
||
EmberNetworkStatus | networkStatus |
||
) |
- Parameters
-
parameters
Current network parameters localEui64
The EUI64 of the Ember chip macExtendedId
The extended MAC ID of the Ember chip networkStatus
The current status of the network
void emberInitReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberInit().
void emberJoinNetworkReturn | ( | EmberStatus | status | ) |
void emberLaunchStandaloneBootloaderReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberLaunchStandaloneBootloader.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure.
void emberLeaderDataHandler | ( | const uint8_t * | leaderData | ) |
- Parameters
-
leaderData
the leader data
bool emberMacPassthroughFilterHandler | ( | uint8_t * | macHeader | ) |
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_MAC_PASSTHROUGH_FILTER_HANDLER
- Parameters
-
macHeader
A pointer to the initial portion of the incoming MAC header, in the standard 802.15.4 format. The first two bytes comprise the frame control, which dictates source / destination PAN and addressing formats. (See the MAC sublayer definition in the standards definition 802.15.4e/2012)
The relevant bytes of the header are:
| octets: | 2 | 1 | 0/2 | 0/2/8 | 0/2 | 0/2/8 |
| | ctl | seq | dst.pan | dst.addr | src.pan | src.addr | ...
Note that subsequent MAC fields, and the MAC payload, may not yet be present at this point.
- Returns
- true if the message is an application MAC passthrough message.
void emberMacPassthroughMessageHandler | ( | PacketHeader | header | ) |
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_MAC_PASSTHROUGH_MESSAGE_HANDLER
- Parameters
-
header
The message buffer pointing to the full 802.15.4 frame to be handled by the application.
bool emberMacRssiFilterHandler | ( | uint8_t * | macHeader | ) |
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_RSSI_FILTER_HANDLER
- Parameters
-
macHeader
A pointer to the initial portion of the incoming MAC header, in the standard 802.15.4 format. The first two bytes comprise the frame control, which dictates source / destination PAN and addressing formats. (See the MAC sublayer definition in the standards definition 802.15.4e/2012)
The relevant bytes of the header are:
| octets: | 2 | 1 | 0/2 | 0/2/8 | 0/2 | 0/2/8 |
| | ctl | seq | dst.pan | dst.addr | src.pan | src.addr | ...
Note that subsequent MAC fields, and the MAC payload, may not yet be present at this point.
- Returns
- true if the application wants to peek at the RSSI for this message.
void emberMacRssiHandler | ( | int8_t | currentRssi | ) |
- Note
- This is called on the application for all packets that match the rule defined in emberMacRssiFilterHandler()
The quantity referenced by currentRssi will contain the energy level (in units of dBm) observed during the last 802.15.4 packet received in that handler.
- Note
- This API is for SoCs only.
- The application must define EMBER_APPLICATION_HAS_RSSI_FILTER_HANDLER
- This functionality is not available for packets such as 802.15.4 data requests or acknowledgements. Data requests must be handled quickly due to strict 15.4 timing requirements, and so the RSSI information is not recorded. Similarly, 802.15.4 ACKs are handled by the hardware and the information does not make it up to the stack.
- Parameters
-
currentRssi
The RSSI for the last incoming message processed.
void emberMicroBusyHandler | ( | bool | busy | ) |
This callback is not available on a host processor. Note that if ::busy is true, the micro may become busy as soon as this handler exits. In a host/ncp setup, one solution for informing the host is to implement this handler in your own xNCP image and use it to toggle the serial CTS line.
void emberNetworkDataChangeHandler | ( | const uint8_t * | networkData, |
uint16_t | length |
||
) |
This function is called when the stack receives new Thread Network Data. The networkData argument may be NULL, in which case emberGetNetworkData can be used to obtain the new Thread Network Data.
- Parameters
-
networkData
the Network Data length
length in bytes of the Network Data
void emberNetworkStatusHandler | ( | EmberNetworkStatus | newNetworkStatus, |
EmberNetworkStatus | oldNetworkStatus, |
||
EmberJoinFailureReason | reason |
||
) |
This function reports a change to the network status. For example, the network status changes while going through the joining process, or while reattaching to the network, which can happen for a variety of reasons. In particular, after issuing a form, join, resume, or attach command, the application knows that the device is on the network and ready to communicate when this handler is called with a newNetworkStatus of EMBER_JOINED_NETWORK_ATTACHED.
If the status handler is reporting a join failure, then the newNetworkStatus argument will have a value of EMBER_NO_NETWORK and the reason argument will contain an appropriate value. For other network status reports, the reason argument does not apply and is set to EMBER_JOIN_FAILURE_REASON_NONE.
void emberOkToNapReturn | ( | uint8_t | stateMask | ) |
The mask EMBER_HIGH_PRIORITY_TASKS defines which tasks are high priority. Devices should not sleep if any high priority tasks are active. Active tasks that are not high priority are waiting for messages to arrive from other devices. If there are active tasks, but no high priority ones, the device may sleep but should periodically wake up and call emberPollForData() in order to receive messages. Parents will hold messages for EMBER_INDIRECT_TRANSMISSION_TIMEOUT (in quarter seconds) before discarding them.
- Returns
- A bitmask of the stack's active tasks.
void emberOpenDtlsConnectionReturn | ( | uint32_t | result, |
const EmberIpv6Address * | remoteAddress, |
||
uint16_t | localPort, |
||
uint16_t | remotePort |
||
) |
- Parameters
-
result
error code - an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
remoteAddress
IPv6 address of the server localPort
local port remotePort
remote port
void emberPollForDataReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberPollForData().
- Parameters
-
An
EmberStatus value: - EMBER_SUCCESS - The poll message has been submitted for transmission
- EMBER_INVALID_CALL - The node is not a sleepy end device.
- EMBER_NOT_JOINED - The node is not part of a network.
void emberProcessCoap | ( | const uint8_t * | message, |
uint16_t | messageLength, |
||
EmberCoapRequestInfo * | info |
||
) |
This function processes a CoAP message received over an alternate transport.
Called to process a CoAP message that arrived via DTLS or other alternative transport. Only the address, port and transmit handler fields of info
are used. The token and ackData fields are ignored.
void emberRadioGetRandomNumbersReturn | ( | EmberStatus | status, |
const uint16_t * | rn, |
||
uint8_t | count |
||
) |
This function provides the result of a call to emberRadioGetRandomNumbers
.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure. When EMBER_SUCCESS is returned ::rn and ::count will contain valid data. ::rn and ::count are undefined when EMBER_SUCCESS is not returned. rn
the uint16_t random values count
- the count of uint16_t values located at ::rn
void emberRequestDhcpAddressReturn | ( | EmberStatus | status, |
const uint8_t * | prefix, |
||
uint8_t | prefixLengthInBits |
||
) |
This function provides the result of a call to emberRequestDhcpAddress.
This call only indicates the status of the request (EMBER_ERR_FATAL if no DHCP server is found, and EMBER_SUCCESS otherwise). The assigned IPv6 address is returned via emberAddressConfigurationChangeHandler
- Parameters
-
status
Status of DHCP Address Request prefix
Prefix requested in emberRequestDhcpAddress prefixLengthInBits
Prefix length in bits requested in emberRequestDhcpAddress
void emberRequestSlaacAddressReturn | ( | EmberStatus | status, |
const uint8_t * | prefix, |
||
uint8_t | prefixLengthInBits |
||
) |
This function provides the result of a call to emberRequestSlaacAddress.
This call only indicates the status of the request (EMBER_ERR_FATAL if no SLAAC server is found, and EMBER_SUCCESS otherwise). The assigned IPv6 address is returned via emberAddressConfigurationChangeHandler
- Parameters
-
status
Status of SLAAC Address Request prefix
Prefix requested in emberRequestSlaacAddress prefixLengthInBits
Prefix length in bits requested in emberRequestSlaacAddress
void emberResetCounterHandler | ( | EmberCounterType | type | ) |
The application must define EMBER_APPLICATION_HAS_COUNTER_VALUE_HANDLER in its CONFIGURATION_HEADER to use this.
- Parameters
-
type
The type of the event.
void emberResetMicroHandler | ( | EmberResetCause | cause | ) |
This function notifies the application of a reset on the Ember chip due to the indicated cause.
void emberResetNetworkStateReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberResetNetworkState().
void emberResignGlobalAddressReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberResignGlobalAddress().
void emberResumeNetworkReturn | ( | EmberStatus | status | ) |
void emberScanReturn | ( | EmberStatus | status | ) |
This function provides the status upon completion of a scan.
void emberSendSteeringDataReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSendSteeringData().
void emberSetAddressHandler | ( | const uint8_t * | address | ) |
A callback that is generated when the host's address changes.
- Parameters
-
address
IP address, 16 bytes
void emberSetAntennaModeReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetAntennaMode
.
- Parameters
-
EMBER_SUCCESS
if antenna mode is configured as desired or EMBER_BAD_ARGUMENT if antenna mode is not supported.
void emberSetCcaThresholdReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetCcaThreshold().
void emberSetCommissionerKeyReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetCommissionerKey(): either EMBER_SUCCESS or EMBER_INVALID_CALL.
void emberSetCtuneReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetCtune.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure.
void emberSetDtlsDeviceCertificateReturn | ( | uint32_t | result | ) |
- Parameters
-
result
- ::0 The certificate was set successfully.
- ::result error code
- an EmberStatus value if using Silicon Labs TLS
- an mbed TLS error code if using mbed TLS library (see mbedtls:include/mbedtls/ssl.h)
void emberSetDtlsPresharedKeyReturn | ( | EmberStatus | status | ) |
- Parameters
-
result
- ::status An EmberStatus value
void emberSetJoinKeyReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetJoinKey().
void emberSetLocalNetworkDataReturn | ( | EmberStatus | status, |
uint16_t | length |
||
) |
Provides the result of a call to ::emberSetServerNetworkData.
void emberSetMfgTokenReturn | ( | EmberMfgTokenId | tokenId, |
EmberStatus | status |
||
) |
This function provides the result of a call to emberSetMfgToken.
- Parameters
-
tokenId
Which manufacturing token set. status
An EmberStatus value indicating success or the reason for failure.
void emberSetNdDataReturn | ( | EmberStatus | status, |
uint16_t | length |
||
) |
This function provides the result of a call to emberSetNdData.
void emberSetPskcHandler | ( | const uint8_t * | pskc | ) |
- Parameters
-
pskc
PSKc: 16 bytes in length
void emberSetPtaEnableReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetPtaEnable
.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure.
void emberSetPtaOptionsReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetPtaOptions
.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure.
void emberSetPtaPwmOptionsReturn | ( | EmberStatus | status | ) |
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure.
void emberSetRadioHoldOffReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetRadioHoldOff
.
- Parameters
-
status
An EmberStatus value indicating success or the reason for failure. EMBER_SUCCESS if Radio HoldOff was configured as desired or EMBER_BAD_ARGUMENT if requesting it be enabled but RHO has not been configured by the BOARD_HEADER.
void emberSetRadioPowerReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetRadioPower() on the host.
void emberSetSecurityParametersReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetSecurityParameters().
void emberSetTxPowerModeReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSetTxPowerMode() on the host.
void emberSlaacServerChangeHandler | ( | const uint8_t * | prefix, |
uint8_t | prefixLengthInBits, |
||
bool | available |
||
) |
This function is called when the stack knows about a new SLAAC prefix or if a SLAAC server has become unavailable.
"available" means we can configure a SLAAC address.
- Parameters
-
prefix
SLAAC prefix prefixLengthInBits
length in bits of the prefix available
whether we can configure an address
void emberStackPollForDataReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberStackPollForData().
void emberStartHostJoinClientHandler | ( | const uint8_t * | parentAddress | ) |
A callback to tell the host to start security commissioning.
- Parameters
-
address
parent IP address, 16 bytes
void emberStateReturn | ( | const EmberNetworkParameters * | parameters, |
const EmberEui64 * | localEui64, |
||
const EmberEui64 * | macExtendedId, |
||
EmberNetworkStatus | networkStatus |
||
) |
- Parameters
-
parameters
Current network parameters localEui64
The EUI64 of the Ember chip macExtendedId
The extended MAC ID of the Ember chip networkStatus
The current status of the network
void emberSwitchToNextNetworkKeyHandler | ( | EmberStatus | status | ) |
This function can be stubbed out on the SoC and host app. It is used by the NCP to update security on the driver when it is instructed to switch the network key by an over the air update.
void emberSwitchToNextNetworkKeyReturn | ( | EmberStatus | status | ) |
This function provides the result of a call to emberSwitchToNextNetworkKey().