Building and Sending Messages#

Commands for building and sending messages out onto the network.

Macros#

#define

interpan group [groupId:2] [destPan:2] [destprofileID:2]

#define

interpan long [longId:8] [destPAN:2] [destProfileID:2] [options:2]

#define

interpan short [shortId:2] [destPan:2] [destprofileID:2]

#define
#define

send [id:2] [src-endpoint:1] [dst-endpoint:1]

#define

send-using-multicast-binding [useMulticastBinding:1]

#define

send_multicast [groupId:2] [src-endpoint:1]

#define

timesync [id:2] [srcEndpoint:1] [destEndpoint:1]

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_BSEND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_BSEND

bsend [srcEndpoint:1]

  • Send using a binding based on the clusterId in the globalApsFrame and the srcEndpoint specified (if the src endpoint is zero it only sends based on the clusterId)

    • srcEndpoint - INT8U - Source endpoint to send a binding based message from


Definition at line 59 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_GROUP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_GROUP

interpan group [groupId:2] [destPan:2] [destprofileID:2]

  • send an interpan message to a group id.

    • groupId - INT16U - group id to send to

    • destPan - INT16U - destination pan id

    • destprofileID - INT16U - destination profile ID


Definition at line 67 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_LONG#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_LONG

interpan long [longId:8] [destPAN:2] [destProfileID:2] [options:2]

  • Send an interpan message to a long address (8 byte eui64)

    • longId - IEEE_ADDRESS - long ieee address to send the interpan message to

    • destPAN - INT16U - two byte destination PA ID

    • destProfileID - INT16U - two byte destination profile ID

    • options - INT16U - two byte options


Definition at line 76 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_SHORT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_INTERPAN_SHORT

interpan short [shortId:2] [destPan:2] [destprofileID:2]

  • Send an interpan message to a short id.

    • shortId - INT16U - group id to send to

    • destPan - INT16U - destination pan id

    • destprofileID - INT16U - destination profile ID


Definition at line 84 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_RAW#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_RAW

raw [clusterId:2] [data:-1]

  • Creates a message by specifying the raw bytes. Use "send" to send the message once it has been created. Ex: raw 0x000F {00 0A 00 11 22 33 44 55} sends a message to cluster 15 (0x000F) of length 8 which includes the ZCL header.

    • clusterId - INT16U - two byte cluster id

    • data - OCTET_STRING - ZCL message, including ZCL header and payload


Definition at line 91 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND

send [id:2] [src-endpoint:1] [dst-endpoint:1]

  • Send a pre-buffered message from a given endpoint to an endpoint on a device with a given short address.

    • id - INT16U - short id of the device to send the message to

    • src-endpoint - INT8U - The endpoint to send the message from

    • dst-endpoint - INT8U - The endpoint to send the message to


Definition at line 99 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_USING_MULTICAST_BINDING#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_USING_MULTICAST_BINDING

send-using-multicast-binding [useMulticastBinding:1]

  • When sending using a binding, specify whether a multicast binding should be used.

    • useMulticastBinding - BOOLEAN - Whether to send via a multicast binding


Definition at line 105 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_MULTICAST#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_SEND_MULTICAST

send_multicast [groupId:2] [src-endpoint:1]

  • Send a pre-buffered multicast message to a given group id from a given endpoint.

    • groupId - INT16U - group id of the multicast group to send the message to

    • src-endpoint - INT8U - The endpoint to send the message from


Definition at line 112 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_TIMESYNC#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_BUILD_SEND_MSG_TIMESYNC

timesync [id:2] [srcEndpoint:1] [destEndpoint:1]

  • This sends a read attr for the time of the device specified. It sets a flag so when it gets the response it writes the time to its own time attr

    • id - INT16U - two byte short id of the time server

    • srcEndpoint - INT8U - source endpoint to send time sync from

    • destEndpoint - INT8U - destination endpoint to expect response on


Definition at line 120 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc