Plugin Commands: Delayed join#
The Delayed join plugin contributes several CLI commands to the application framework to be used in handlying delayed join and sending the network key.
Macros#
plugin delayed-join activate
plugin delayed-join send-network-key [nodeId:2] [EUI64:8] [parentNodeId:2] [newKey:-1]
plugin delayed-join set-key-timeout [seconds:1]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DELAYED_JOIN_PLUGIN_DELAYED_JOIN_ACTIVATE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DELAYED_JOIN_PLUGIN_DELAYED_JOIN_ACTIVATE
plugin delayed-join activate
Sets the TC join policy to delayed-join
2481
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DELAYED_JOIN_PLUGIN_DELAYED_JOIN_SEND_NETWORK_KEY#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DELAYED_JOIN_PLUGIN_DELAYED_JOIN_SEND_NETWORK_KEY
plugin delayed-join send-network-key [nodeId:2] [EUI64:8] [parentNodeId:2] [newKey:-1]
Triggers sending the encrypted network key to the joining node
nodeId - INT16U - Short address of the key destination
EUI64 - IEEE_ADDRESS - Long address of the key destination
parentNodeId - INT16U - address of the key destination
newKey - OCTET_STRING - The network key
2490
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DELAYED_JOIN_PLUGIN_DELAYED_JOIN_SET_KEY_TIMEOUT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_DELAYED_JOIN_PLUGIN_DELAYED_JOIN_SET_KEY_TIMEOUT
plugin delayed-join set-key-timeout [seconds:1]
Extends the joiner timeout to wait for the network key during join
seconds - INT8U
2496
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc