Plugin Commands: Update TC Link Key#

The update trust center link key commands are used to manipulate the behavior of the joining device to attempt the trust center link key updates in a certain fashion.

Macros#

#define

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_UPDATE_TC_LINK_KEY_PLUGIN_UPDATE_TC_LINK_KEY_TIMER

plugin update-tc-link-key timer [timeInMilliseconds:4]

  • This sets the the amount of time between subsequent trust center link key updates in milliseconds.

    • timeInMilliseconds - INT32U - The amount of time between subsequent trust center link key updates in milliseconds


Definition at line 7130 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc