Plugin Commands: Manufacturing Library#

CLI commands related to the manufacturing library.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_LOCK#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_LOCK

plugin configuration-server lock [lock:1]

  • Lock/unlock the configuration cluster.

    • lock - BOOLEAN - True means lock, false means unlock.


Definition at line 3913 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_READ#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_READ

plugin configuration-server read

  • Read a token supported by the configuration server.


Definition at line 3918 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_SET#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_CONFIGURATION_SERVER_PLUGIN_CONFIGURATION_SERVER_SET

plugin configuration-server set [creator:2] [data:-1]

  • Set a token supported by the configuration server.

    • creator - INT16U - True means lock, false means unlock.

    • data - OCTET_STRING - Data to use to write the token.


Definition at line 3925 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc