Plugin Commands: EZ-Mode Commissioning#
The EZ-Mode Commissioning plugin contributes several commands to the application framework's CLI.
Macros#
plugin ezmode-commissioning client [endpoint:1] [direction:1] [clusterIds:2]
plugin ezmode-commissioning server [endpoint:1] [identifyTimeS:2]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_CLIENT
plugin ezmode-commissioning client [endpoint:1] [direction:1] [clusterIds:2]
Start EZ-Mode client commissioning.
endpoint - INT8U - The local endpoint.
direction - INT8U - ::EMBER_AF_EZMODE_COMMISSIONING_SERVER_TO_CLIENT or ::EMBER_AF_EZMODE_COMMISSIONING_CLIENT_TO_SERVER.
clusterIds - INT16U - A list of cluster ids.
2963
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_EZMODE_COMMISSIONING_PLUGIN_EZMODE_COMMISSIONING_SERVER
plugin ezmode-commissioning server [endpoint:1] [identifyTimeS:2]
Start EZ-Mode server commissioning.
endpoint - INT8U - The local endpoint.
identifyTimeS - INT16U - The identify time in seconds.
2970
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc