Plugin Commands: Meter Snapshot Server#
The meter-snapshot-server plugin contributes several commands to the application framework's CLI. These commands are used for taking and publishing snapshots.
Macros#
plugin meter-snapshot-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [startTime:4] [endTime:4] [offset:1] [cause:4]
plugin meter-snapshot-server take [endpoint:1] [cause:4]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_PUBLISH#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_PUBLISH
plugin meter-snapshot-server publish [nodeId:2] [srcEndpoint:1] [dstEndpoint:1] [startTime:4] [endTime:4] [offset:1] [cause:4]
Publish a snapshot.
nodeId - INT16U - the destination node id
srcEndpoint - INT8U - the source endpoint
dstEndpoint - INT8U - the destination endpoint
startTime - INT32U - the earliest time of a snapshot to be published
endTime - INT32U - the latest time of a snapshot to be published
offset - INT8U - identifies the snapshot to be published
cause - INT32U - select only snapshots that were taken due to a specific cause
4221
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_TAKE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_METER_SNAPSHOT_SERVER_PLUGIN_METER_SNAPSHOT_SERVER_TAKE
plugin meter-snapshot-server take [endpoint:1] [cause:4]
Take a snapshot.
endpoint - INT8U - the source endpoint
cause - INT32U - the cause of the snapshot
4228
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc