Plugin Commands: Comms Hub Function (SubGhz)#
Macros#
#define
plugin comms-hub-function-sub-ghz channel-change-complete [page:1] [channel:1]
#define
plugin comms-hub-function-sub-ghz channel-change-start
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_COMPLETE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_COMPLETE
plugin comms-hub-function-sub-ghz channel-change-complete [page:1] [channel:1]
Complete the channel change sequence.
page - INT8U - Requested new page [28-31]
channel - INT8U - Requested new channel
Definition at line
2152
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_START#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_PLUGIN_COMMS_HUB_FUNCTION_SUB_GHZ_CHANNEL_CHANGE_START
plugin comms-hub-function-sub-ghz channel-change-start
Initiate the channel change sequence.
Definition at line
2157
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc