Plugin Commands: Multi-Network Price Passthrough#

The Multi-Network Price Passthrough plugin is a plugin designed to demonstrate multi-network functionality by passing data from a "real" ESI on one network to a "proxy" ESI on another network via periodic polling and forwarding.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_PRINT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_PRINT

plugin mn-price-passthrough print

  • Print the current price known to the proxy esi.


Definition at line 4245 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_SET_ROUTING#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_SET_ROUTING

plugin mn-price-passthrough set-routing [fwdId:2] [fwdEndpoint:1] [esiEndpoint:1]

  • Set the routing parameters.

    • fwdId - INT16U - The node id of the forwarding endpoint.

    • fwdEndpoint - INT8U - The forwarding endpoint.

    • esiEndpoint - INT8U - The endpoint of the proxy ESI.


Definition at line 4253 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_START#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_START

plugin mn-price-passthrough start

  • Starts polling and forwarding.


Definition at line 4258 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_STOP#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_MN_PRICE_PASSTHROUGH_PLUGIN_MN_PRICE_PASSTHROUGH_STOP

plugin mn-price-passthrough stop

  • Stops polling and forwarding.


Definition at line 4263 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc