Plugin Commands: Slot Manager#
This plugin provides a set of CLI commands to interact with external SPI flash, particularly in a setup where slots are present to work with the common bootloader.
Macros#
plugin slot-manager boot-slot [slotId:4]
plugin slot-manager erase-slot [slotId:4]
plugin slot-manager ext-flash-info
plugin slot-manager read [address:4] [length:1]
plugin slot-manager slots-info
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_BOOT_SLOT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_BOOT_SLOT
plugin slot-manager boot-slot [slotId:4]
Boot the image in the specified slot ID.
slotId - INT32U - The slot ID to boot
6283
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_ERASE_SLOT#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_ERASE_SLOT
plugin slot-manager erase-slot [slotId:4]
Erase the specified slot ID.
slotId - INT32U - The slot ID to erase
6289
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_EXT_FLASH_INFO#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_EXT_FLASH_INFO
plugin slot-manager ext-flash-info
Print external flash information.
6294
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_READ#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_READ
plugin slot-manager read [address:4] [length:1]
Read raw data from external flash.
address - INT32U - Address to read
length - INT8U - Length of bytes to read
6301
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_SLOTS_INFO#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_SLOT_MANAGER_PLUGIN_SLOT_MANAGER_SLOTS_INFO
plugin slot-manager slots-info
Print information for all available slots.
6306
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc