Plugin Commands: Trust Center Backup#

The Trust Center Backup plugin contributes several CLI commands to the application framework to be used in creating and managing reporting table entries directly on the device.

Macro Definition Documentation#

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_CLEAR_IMPORT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_CLEAR_IMPORT

plugin trust-center-backup clear-import

  • Clear the import data set.


Definition at line 7000 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_IMPORT_KEY#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_IMPORT_KEY

plugin trust-center-backup import-key [index:1] [partnerEUI64:8] [newKey:-1]

  • Set a key in the import data set.

    • index - INT8U

    • partnerEUI64 - IEEE_ADDRESS

    • newKey - OCTET_STRING


Definition at line 7024 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_EXPORT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_EXPORT

plugin trust-center-backup print-export

  • Print the set of export data that a TC must backup.


Definition at line 7029 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_IMPORT#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_PRINT_IMPORT

plugin trust-center-backup print-import

  • Print the import data set.


Definition at line 7034 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_RESTORE#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_RESTORE

plugin trust-center-backup restore

  • Use the import data set in a restore operation to bring the TC back online.


Definition at line 7039 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc

EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_SET_EXT_PAN#

#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_TRUST_CENTER_BACKUP_PLUGIN_TRUST_CENTER_BACKUP_SET_EXT_PAN

plugin trust-center-backup set-ext-pan [extendedPanId:8]

  • Set the extended PAN ID in the import data set.

    • extendedPanId - IEEE_ADDRESS


Definition at line 7045 of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc