Plugin Commands: Wwah Server#
The wwah-server plugin contributes CLI commands to the application framework to be used for printing information related to the WWAH server.
Macros#
plugin wwah-server confMode [mode:1]
plugin wwah-server poweringOff [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]
plugin wwah-server poweringOn [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]
Macro Definition Documentation#
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_CONF_MODE#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_CONF_MODE
plugin wwah-server confMode [mode:1]
Set the configurationModeEnabled attribute command.
mode - INT8U - The wwah server configuration mode attribute
7191
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_OFF#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_OFF
plugin wwah-server poweringOff [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]
Send the Powering Off Notification command.
srcEndpoint - INT8U - The wwah server (source) endpoint
dstEndpoint - INT8U - The wwah client (dest) endpoint
reason - INT8U - The cause of the power off event
mfgId - INT16U - The manufacturerId of the sender
7200
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc
EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_ON#
#define EMBER_AF_DOXYGEN_CLI_COMMAND_PLUGIN_WWAH_SERVER_PLUGIN_WWAH_SERVER_POWERING_ON
plugin wwah-server poweringOn [srcEndpoint:1] [dstEndpoint:1] [reason:1] [mfgId:2]
Send the Powering On Notification command.
srcEndpoint - INT8U - The wwah server (source) endpoint
dstEndpoint - INT8U - The wwah client (dest) endpoint
reason - INT8U - The cause of the power on event
mfgId - INT16U - The manufacturerId of the sender
7209
of file /Users/vihuszar/Git/EmbeddedSoftware/super/protocol/zigbee/app/framework/test/headers/cli.doc